Need rotary Pot with rotary switch

I have been looking all over DigiKey and Mouser as well as doing some google searches, but I cannot find a rotary potentiometer with a rotary switch and 1/8” shaft along with being PCB mounted with vertical pins that is reasonably priced.
All I can find is this Bourns 39SB-1RB-103 that is priced at 30.00.
Is that the best I can do? I hate to spend that much on a pot since I need two of them.
I need them to emulate these on a KX-155 radio that is similar to the image I am building for my flight sim. They do not need the push / pull switch function. Although the one on the left would be nice to have the on /off switch.
I have limited space on the PCB so a diameter around 12 mm similar to the Bourns I mentioned will work best.
But I guess if the Bourns pot is all I can get then so be it.

Hello, Roger.

Would 3310H-003-103L work for your requirement?