I have removed a flexible COB LED strip from a Artika brand ceiling light fixture and the driver ar the housing has the following specs; lin 0.4A max VOut 30-39VDC lOut 600mA C.C. Max POut 23.4 W pF>0.92
on the LED strip has marking as 2835 100mm 13C
I have looked at the catalog, but can not find the right one, is anyone able to help me finding it please.
Thanks in advance
Hello buildwrightcustom,
I was unable to find a 100mm strip LED, to match the output current and voltage.
The closest items to handle the 600mA, Constant Current output, with a voltage range of 30-39VDC, and 24mm X 20mm COBs. Here is a link to those options: LED COBs, Engines, Modules, Electronic Components Distributor DigiKey
Thank you David, appreciated, even though it is printed as 100 mm, each LED measures like the dimensions you have suggested: 24x 20mm. The white base measures 100 mm.
I have looked at your list and I assume I would need the tube version rather than the tray, I am confused about the price though, does each LED count as a unit?
Regards