Discontinued LED CoBs

Hello all,
I am searching for a replacement LED CoB to rebuild the LED overheads lights in the crew cabins onboard our vessel. Built originally in The Netherlands. Original: 230vac to 24 vdc dimming module to constant current driver to Cob.
I would much rther build my own unit rather than convert to the newer all in one g4 plug ins.

The original CoBs had a fwd voltage of 14vdc, ±1klm, fwd current 700mA, 3000k, macadam 5.

The closet I have found on Digikey with firstly the correct fwd voltage is the :CDM-6-3018-90-18-DW02

Seems this will work and also physically fit into the same area needed. My only reservation is that even though the Kelvin is 3k the luminous flux is roughly half.

Given the kelvin is the same, how much would the lm be noticable beside the original?

Any assistance is greatly appreciated. Thanks

Welcome to the community!

A 50% reduction in luminous flux would create a distinct difference in the lighting output. I see looking at the specs for CDM-6-3018-90-18-DW02 that it can be driven at a max of 440mA. Driving at that current would result in a higher lm output but the overall operating life of the LEDs would decrease.

We do have other options at 35.5V @ 300mA in the same LED series that have higher lm output here if you can design around those specs.

Hello sir,

Thank you sir! I’m glad to be a part of it!

Ok understood thank you, very much for the clarification.

I will give these a look over. I see what you’re saying. And yes I believe one of these will be the best option.

CDM-9-3018-90-36-DW01 This one specifically, I’ll ensure I can get some more voltage out of the dimming modules.

Thanks so much for your help, I’m not a fan of replacing with g4s just because it’s easier haha

Also sir,
With this CoB module mentioned, before this component, the constant current driver is rated for 10-35vdc, which checks with the chart, then constant current is 350mA.
With this module: CDM-9-3018-90-36-DW01, I should be fine with leaving the constant current drivers that are in place now? Or find a more suitable range for these as well?

The constant current driver would be on the edge of what it can provide for the LED. The typical forward voltage of the led is 35.5V and has a current test of 300mA with a maximum current of 440mA. Driving at 350mA would be fine, I’m just not sure if being that close to the edge of the typical voltage if the driver is going to be sufficient to drive the LED. You could test the LED but I can’t make any guarantees that the driver will work properly with the part.

Understood sir, thank you for the explanation, its a bit confusing how all these parameters work together for me so thank you for the clarification. Your information has definitely given me several directions to run.

This post speaks to the business of picking a driver suitable for a given LED. Apologies for busted links (it’s ~10 year old content…) but the general ideas remain valid. Note that if you’re matching an LED to a driver, you’d need to work in a somewhat different direction.

That said…

These LED ratings would mean that if a person shoves 700mA of current through the device, about 1000lm of light will come out, and one will need about 14V available in order to get the specified 700mA to flow.

Note that 0.7A*14V=9.8 watts of power, roughly half of which would have ended up getting turned into heat instead of light.

A driver specification like that means a device that is designed to shove 350mA through whatever is connected to it, and not complain so long as the voltage required to do that ends up somewhere between 10 and 35V.

In other words, while the old LEDs might have been rated for 700mA, they would have only been operated at 350mA. Lumen output (i.e. total quantity of light) is pretty much proportional to drive current, so an LED rated for 1000lm @ 700mA would only be delivering ~500lm @ 350mA.

Also, it would only be giving off half the amount of heat @ 350mA that it would if run @ 700mA. That’s important, because LEDs very much do not like heat/temperature.

If we look at the specs for the CDM-9-3018-90-36-DW01, we find a test current figure as well as a max current figure. The flux rating and forward voltage apply at the specified test current and temperature.

If you tried to run that LED at 350mA instead of 300, the forward voltage is going to be a tad higher and pushing slightly beyond the stated limits of your driver. (The relationship between voltage and current is not proportional, which is why we have to mess around with constant-current drivers…)

Under those conditions, one would anticipate slightly north of 1000lm out of the device, which is roughly twice the light one would have actually been getting out of the old setup. Additionally, the total power burn would be roughly 0.35A*36V = 12.6W, roughly 2.5x more than original.

What I’m getting at here is that the CDM-6-3018-90-18-DW02 originally mentioned is probably the better option of those discussed so far. Light output should be roughly comparable, and while the power burn/heat output would be slightly higher than the original, it’s 'aint no 2.5x higher.

Part of the reason this CoB is less efficient than some is that it does a bunch of fancy gizzyfritzing to end up with a light color that shifts more red/yellow as it dims, like an old-fashioned incandescent did. It also goes to some pains to produce light that doesn’t do odd things from a color perception perspective. (CRI=Color Rendering Index: higher=less funny business, lower usually=more lumens/watt, all else equal)

My suggestion to you would be to clarify what’s tolerable from a mechanical mounting standpoint, and where you’d like to go from a color temperature standpoint. Higher color temperature (CCT) are called “cool” and are more blue, lower CCTs are called “warm”, are more yellow, and deliver less light/watt in general. Pretty much a preference thing.

There’s actually a few hundred part numbers in stock that would seem in-ballpark from an electrical standpoint once a person figures for the whole operating-point business, once a person figures for the whole rated-for versus operated-at business…

Good morning Rick,
This is a wonderful explanation, thank you very much for this. Its ridiculous how much more this makes sense to me with this. Understood. Ive ordered several different options to try out in my cabin. Captain is fine as long as I can get close to the Kelvin and lm. Specifically of the one youve mentioned Ive gotten myself a couple options.

Wanted to say I appreciate your time. ive opened the rabbit hole and am currently learning of the covalent bonds being broken to create the photon in the first place, and the means we have to manipulate it.

Thanks to all

1214-1554-ND
These worked perfectly, I was able to adjust the fwd voltage and even out the lm to match perfectly with existing. Thanks again. Now on to NPA pressure sensors!

Hello @Taylor764

We are glad to hear that 1214-1554-ND worked perfectly for you and let us know if you need any help in find a NPA pressure sensor