Numero de parte Conector de Antena Celular

Hi cvega,

Here’s another link which should get you to our selection of SMA receptacle options.

Things to note:

  • Your footprint is pretty universal for the four-pin right angle SMA connectors, so we have many parts which meet that requirement.
  • The connector face for an SMA jack/receptacle (the terms are synonymous) are standardized at 1/4"-36 UNS-2A, so all of these will also meet that requirement.

What is not standardized are the following:

  • Other connector dimensions
  • Internal and external materials used
  • Frequency capabilities (for example, the max frequency for SMA connectors in link provided range from 2 GHz to 20 GHz)
  • Different ingress ratings (ranging from unrated to the water-proof IP69K)

If you need an exact physical match, we may not have a match for you, but if you have some flexibility, then one or more of these may work.

Just looking through parts in the link, the 0732515490, the 901-10138, and the 142-0711-531 seem to be some of the closer physical matches, though not identical.

1 Like