We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I bought a 4G LTE antenna for my caravan and I want to mount it outside. I need a new cable as the one I have now is not long enough. Also I would need to cut the plugs off in order to pull the cable thru.
I don’t have much technical specifications to go on but maybe I can get some help here. The cable is marked “LL58”. In addition to more cable (<6m / 20feet) I need cable to male connector and female-to-female SMA connector as I would need to splice two cables at some point.
Does DigiKey have this? I cant find “LL58” but what “RG” group is similar? Also some fitting SMA connectors
Aside from having appropriate connectors, using a cable with the correct characteristic impedance (50 ohms most likely) is the thing to look for. The “LL58” cable mentioned seems likely to be of the RG58 style.
Matching the choice of a connector part number to an appropriate cable style is needed, as 50 ohm coaxial cables can vary widely in size. Many user-applied coaxial connectors require a specialized crimp tool which can be costly. There are some such as P/N 132125 which can be applied without using such a tool however, which might be a good choice if only a few are needed.
And yes, the LMR-240 cable product mentioned is sold as a custom-length material; ordering Qty 32 will get you a 32-foot long length of product.