Hello,
after proceeding twice with https://www.digikey.com/eewiki/display/linuxonarm/PandaBoard I don’t have any network connectivity (neither eth0 nor wlan0). Had anyone simmilar problem? I have checked on two boards (we have couple of them in office). Also Ubuntu 18.01 is using netplan (not ifupdown).
Br,
Marek
@marverix, which kernel are you currently using? Did the smsc95xx usb module load?
Regards,
Hello Robert!
I send email to eewiki@digikey.com but probably didn’t reached you out, so I will paste part of it:
Thank you for great wiki page about PandaBoard! We have in our company couple of them and those were lying without purpouse because lack of software.
I have followed wiki step by step and PandaBoard-ES B3 is booting (finally!), but it doesn’t see any network adapters.
Also one comment: on Ubuntu 18.04.1 (which I’m using) ipdownup is not longer use - they use netplan. I tried both ways, but still nothing.
I have tried twice - first with everything according to Wiki, and second with other (newer) packages (Linaro 7.3.1, U-boot v2019.1, Ubuntu 18.04.1 2018.12.26).
Kernel which I’m using right now is 4.14.x (previously I tried 4.19.x).
Regarding smsc95xx. I’m attaching log from COM1.
U-Boot SPL 2019.01-dirty (Jan 17 2019 - 16:18:45 +0100)
OMAP4460-GP ES1.1
Trying to boot from MMC1
SPL: Please implement spl_start_uboot() for your board
SPL: Direct Linux boot not active!
U-Boot 2019.01-dirty (Jan 17 2019 - 16:18:45 +0100)
CPU : OMAP4460-GP ES1.1
Board: OMAP4 Panda
I2C: ready
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... Unable to use mmc 0:1... Net: No ethernet found.
Press SPACE to abort autoboot in 2 seconds
## Error: "init_console" not defined
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** File not found boot.scr **
** Unrecognized filesystem type **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
Checking for: /uEnv.txt ...
Checking for: /boot/uEnv.txt ...
52 bytes read in 10 ms (4.9 KiB/s)
Loaded environment from /boot/uEnv.txt
Using: dtb=omap4-panda-es-b3.dtb ...
Checking if uname_r is set in /boot/uEnv.txt...
Running uname_boot ...
loading /boot/vmlinuz-4.14.91-armv7-x14 ...
10310144 bytes read in 482 ms (20.4 MiB/s)
loading /boot/dtbs/4.14.91-armv7-x14/omap4-panda-es-b3.dtb ...
90786 bytes read in 166 ms (533.2 KiB/s)
debug: [console=ttyO2,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait] ...
debug: [bootz 0x82000000 - 0x88000000] ...
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe6000, end 8ffff2a1 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.91-armv7-x14 (marverix@blackstorm) (gcc version 7.3.1 20180425 [linaro-7.3-2018.05 revision d29120a424ecfbc167ef90065c0eeb7f91977701] (Linaro GCC 7.3-2018.05)) #1 SMP PREEMPT Thu Jan 17 17:28:24 CET 2019
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=50c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI OMAP4 PandaBoard-ES
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0xbc800000
[ 0.000000] OMAP4: Map 0xbfe00000 to fe600000 for dram barrier
[ 0.000000] OMAP4460 ES1.1
[ 0.000000] random: get_random_bytes called from start_kernel+0x8d/0x37a with crng_init=0
[ 0.000000] percpu: Embedded 18 pages/cpu @ef698000 s41164 r8192 d24372 u73728
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259904
[ 0.000000] Kernel command line: console=ttyO2,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 967468K/1046528K available (10240K kernel code, 1555K rwdata, 4980K rodata, 1024K init, 380K bss, 29908K reserved, 49152K cma-reserved, 210944K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf800000 - 0xbfe00000 ( 6 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0b00000 (11232 kB)
[ 0.000000] .init : 0xc1100000 - 0xc1200000 (1024 kB)
[ 0.000000] .data : 0xc1200000 - 0xc1384f38 (1556 kB)
[ 0.000000] .bss : 0xc138f654 - 0xc13ee710 ( 381 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] ftrace: allocating 44739 entries in 88 pages
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: CPU: 0 PID: 0 at arch/arm/kernel/insn.c:15 __arm_gen_branch+0x7f/0x84
[ 0.000000] Modules linked in:
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 4.14.91-armv7-x14 #1
[ 0.000000] Hardware name: Generic OMAP4 (Flattened Device Tree)
[ 0.000000] [<c010e539>] (unwind_backtrace) from [<c010a609>] (show_stack+0x11/0x14)
[ 0.000000] [<c010a609>] (show_stack) from [<c09f1101>] (dump_stack+0x5d/0x6c)
[ 0.000000] [<c09f1101>] (dump_stack) from [<c0133da3>] (__warn+0xaf/0xc0)
[ 0.000000] [<c0133da3>] (__warn) from [<c0133e65>] (warn_slowpath_null+0x19/0x1c)
[ 0.000000] [<c0133e65>] (warn_slowpath_null) from [<c010da6f>] (__arm_gen_branch+0x7f/0x84)
[ 0.000000] [<c010da6f>] (__arm_gen_branch) from [<c010d9db>] (ftrace_make_nop+0xf/0x24)
[ 0.000000] [<c010d9db>] (ftrace_make_nop) from [<c01c9fd3>] (ftrace_process_locs+0x227/0x2f0)
[ 0.000000] [<c01c9fd3>] (ftrace_process_locs) from [<c1115b3b>] (ftrace_init+0x6b/0xa8)
[ 0.000000] [<c1115b3b>] (ftrace_init) from [<c1100975>] (start_kernel+0x1d7/0x37a)
[ 0.000000] [<c1100975>] (start_kernel) from [<8000807f>] (0x8000807f)
[ 0.000000] ---[ end trace 566d496eef74c670 ]---
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: CPU: 0 PID: 0 at kernel/trace/ftrace.c:2094 ftrace_bug+0x209/0x29c
[ 0.000000] Modules linked in:
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Tainted: G W 4.14.91-armv7-x14 #1
[ 0.000000] Hardware name: Generic OMAP4 (Flattened Device Tree)
[ 0.000000] [<c010e539>] (unwind_backtrace) from [<c010a609>] (show_stack+0x11/0x14)
[ 0.000000] [<c010a609>] (show_stack) from [<c09f1101>] (dump_stack+0x5d/0x6c)
[ 0.000000] [<c09f1101>] (dump_stack) from [<c0133da3>] (__warn+0xaf/0xc0)
[ 0.000000] [<c0133da3>] (__warn) from [<c0133e65>] (warn_slowpath_null+0x19/0x1c)
[ 0.000000] [<c0133e65>] (warn_slowpath_null) from [<c01c9d19>] (ftrace_bug+0x209/0x29c)
[ 0.000000] [<c01c9d19>] (ftrace_bug) from [<c01c9fe5>] (ftrace_process_locs+0x239/0x2f0)
[ 0.000000] [<c01c9fe5>] (ftrace_process_locs) from [<c1115b3b>] (ftrace_init+0x6b/0xa8)
[ 0.000000] [<c1115b3b>] (ftrace_init) from [<c1100975>] (start_kernel+0x1d7/0x37a)
[ 0.000000] [<c1100975>] (start_kernel) from [<8000807f>] (0x8000807f)
[ 0.000000] ---[ end trace 566d496eef74c671 ]---
[ 0.000000] ftrace failed to modify
[ 0.000000] [<c110da48>] omap_vp_init+0x8/0x13e
[ 0.000000] actual: 67:f0:ba:e9
[ 0.000000] Initializing ftrace call sites
[ 0.000000] ftrace record flags: 0
[ 0.000000] (0)
[ 0.000000] expected tramp: c010d801
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=2.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] L2C: platform modifies aux control register: 0x0e070000 -> 0x3e470000
[ 0.000000] L2C: DT/platform modifies aux control register: 0x0e070000 -> 0x3e470000
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] OMAP L2C310: ROM does not support power control setting
[ 0.000000] L2C-310 dynamic clock gating disabled, standby mode disabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x4e470000
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node dss_fck
[ 0.000000] OMAP clockevent source: timer1 at 32768 Hz
[ 0.000000] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[ 0.000030] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.002136] Console: colour dummy device 80x30
[ 0.002136] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.002166] This ensures that you still see kernel messages. Please
[ 0.002166] update your kernel commandline.
[ 0.002197] Calibrating delay loop... 1397.55 BogoMIPS (lpj=6987776)
[ 0.087738] pid_max: default: 32768 minimum: 301
[ 0.088043] Security Framework initialized
[ 0.088043] Yama: becoming mindful.
[ 0.088104] AppArmor: AppArmor initialized
[ 0.088195] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.088226] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.089050] CPU: Testing write buffer coherency: ok
[ 0.089080] CPU0: Spectre v2: using BPIALL workaround
[ 0.089324] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.127777] Setting up static identity map for 0x80100000 - 0x80100054
[ 0.147735] Hierarchical SRCU implementation.
[ 0.171997] EFI services will not be available.
[ 0.187713] smp: Bringing up secondary CPUs ...
[ 0.297729] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.297729] CPU1: Spectre v2: using BPIALL workaround
[ 0.297912] smp: Brought up 1 node, 2 CPUs
[ 0.297912] SMP: Total of 2 processors activated (2795.11 BogoMIPS).
[ 0.297943] CPU: All CPU(s) started in SVC mode.
[ 0.299072] devtmpfs: initialized
[ 0.319152] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.319488] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.319519] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.323638] xor: measuring software checksum speed
[ 0.417724] arm4regs : 1010.800 MB/sec
[ 0.517700] 8regs : 792.800 MB/sec
[ 0.617706] 32regs : 764.400 MB/sec
[ 0.717712] neon : 731.600 MB/sec
[ 0.717712] xor: using function: arm4regs (1010.800 MB/sec)
[ 0.717742] pinctrl core: initialized pinctrl subsystem
[ 0.718353] DMI not present or invalid.
[ 0.718719] NET: Registered protocol family 16
[ 0.721710] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.724395] omap_hwmod: l3_main_3 using broken dt data from ocp
[ 0.726806] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.848602] cpuidle: using governor menu
[ 0.856964] OMAP GPIO hardware version 0.1
[ 0.861694] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.861694] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.882019] No ATAGs?
[ 0.882110] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.882141] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.883239] OMAP DMA hardware revision 0.0
[ 0.899414] raid6: using algorithm neonx8 gen() 0 MB/s
[ 0.899414] raid6: .... xor() 0 MB/s, rmw enabled
[ 0.899444] raid6: using neon recovery algorithm
[ 0.912353] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.997955] reg-fixed-voltage wl12xx_vmmc: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_wl12xx_gpio, deferring probe
[ 1.002655] omap-iommu 4a066000.mmu: 4a066000.mmu registered
[ 1.002929] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 1.005310] SCSI subsystem initialized
[ 1.005737] usbcore: registered new interface driver usbfs
[ 1.005798] usbcore: registered new interface driver hub
[ 1.005889] usbcore: registered new device driver usb
[ 1.007232] omap_i2c 48070000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c1_pins, deferring probe
[ 1.007293] omap_i2c 48072000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c2_pins, deferring probe
[ 1.007324] omap_i2c 48060000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c3_pins, deferring probe
[ 1.007385] omap_i2c 48350000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c4_pins, deferring probe
[ 1.007598] media: Linux media interface: v0.10
[ 1.007629] Linux video capture interface: v2.00
[ 1.007781] pps_core: LinuxPPS API ver. 1 registered
[ 1.007781] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 1.007812] PTP clock support registered
[ 1.007965] dmi: Firmware registration failed.
[ 1.008453] omap-mailbox 4a0f4000.mailbox: omap mailbox rev 0x400
[ 1.009887] NetLabel: Initializing
[ 1.009918] NetLabel: domain hash size = 128
[ 1.009918] NetLabel: protocols = UNLABELED CIPSOv4 CALIPSO
[ 1.010009] NetLabel: unlabeled traffic allowed by default
[ 1.010559] clocksource: Switched to clocksource 32k_counter
[ 1.141479] VFS: Disk quotas dquot_6.6.0
[ 1.141571] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.142181] AppArmor: AppArmor Filesystem Enabled
[ 1.155090] NET: Registered protocol family 2
[ 1.155761] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 1.155853] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 1.156005] TCP: Hash tables configured (established 8192 bind 8192)
[ 1.156127] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 1.156188] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 1.156433] NET: Registered protocol family 1
[ 1.167114] RPC: Registered named UNIX socket transport module.
[ 1.167114] RPC: Registered udp transport module.
[ 1.167144] RPC: Registered tcp transport module.
[ 1.167144] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.170288] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 1.170532] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 1.173858] audit: initializing netlink subsys (disabled)
[ 1.174072] audit: type=2000 audit(1.160:1): state=initialized audit_enabled=0 res=1
[ 1.174926] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 1.180847] zbud: loaded
[ 1.193817] NFS: Registering the id_resolver key type
[ 1.193847] Key type id_resolver registered
[ 1.193878] Key type id_legacy registered
[ 1.193908] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.194091] fuse init (API version 7.26)
[ 1.199096] jitterentropy: Initialization failed with host not compliant with requirements: 2
[ 1.199249] Key type asymmetric registered
[ 1.199249] Asymmetric key parser 'x509' registered
[ 1.199340] bounce: pool size: 64 pages
[ 1.199401] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 1.199584] io scheduler noop registered
[ 1.199584] io scheduler deadline registered
[ 1.199768] io scheduler cfq registered (default)
[ 1.199798] io scheduler mq-deadline registered
[ 1.204803] pinctrl-single 4a100040.pinmux: 203 pins at pa fc100040 size 406
[ 1.205352] pinctrl-single 4a31e040.pinmux: 28 pins at pa fc31e040 size 56
[ 1.221313] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled
[ 1.223907] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 32, base_baud = 3000000) is a 8250
[ 1.224609] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 33, base_baud = 3000000) is a 8250
[ 1.225311] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 34, base_baud = 3000000) is a 8250
[ 2.447509] console [ttyS2] enabled
[ 2.451751] 4806e000.serial: ttyS3 at MMIO 0x4806e000 (irq = 35, base_baud = 3000000) is a 8250
[ 2.464385] omapdss_dss 58000000.dss: 58000000.dss supply vdda_video not found, using dummy regulator
[ 2.473785] DSS: OMAP DSS rev 4.0
[ 2.479919] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 2.488006] OF: graph: no port node found in /ocp/dss@58000000/encoder@58005000
[ 2.495452] omapdss_dss 58000000.dss: bound 58005000.encoder (ops dsi_component_ops)
[ 2.503906] omapdss_dss 58000000.dss: bound 58006000.encoder (ops hdmi4_component_ops)
[ 2.513977] connector-dvi connector0: failed to parse ddc-i2c-bus
[ 2.522613] Error: Driver 'tfp410' is already registered, aborting...
[ 2.534759] usbcore: registered new interface driver dln2
[ 2.545745] libphy: Fixed MDIO Bus: probed
[ 2.555328] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.561920] ehci-platform: EHCI generic platform driver
[ 2.567504] ehci-omap: OMAP-EHCI Host Controller driver
[ 2.593170] ehci-omap 4a064c00.ehci: EHCI Host Controller
[ 2.598602] ehci-omap 4a064c00.ehci: new USB bus registered, assigned bus number 1
[ 2.606475] ehci-omap 4a064c00.ehci: irq 142, io mem 0x4a064c00
[ 2.640624] ehci-omap 4a064c00.ehci: USB 2.0 started, EHCI 1.00
[ 2.646820] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.653686] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.660949] usb usb1: Product: EHCI Host Controller
[ 2.665863] usb usb1: Manufacturer: Linux 4.14.91-armv7-x14 ehci_hcd
[ 2.672271] usb usb1: SerialNumber: 4a064c00.ehci
[ 2.677612] hub 1-0:1.0: USB hub found
[ 2.681457] hub 1-0:1.0: 3 ports detected
[ 2.686889] usbcore: registered new interface driver usb-storage
[ 2.693969] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 2.699768] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 2.707885] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.714721] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.722015] usb usb2: Product: MUSB HDRC host driver
[ 2.727020] usb usb2: Manufacturer: Linux 4.14.91-armv7-x14 musb-hcd
[ 2.733428] usb usb2: SerialNumber: musb-hdrc.1.auto
[ 2.738952] hub 2-0:1.0: USB hub found
[ 2.742767] hub 2-0:1.0: 1 port detected
[ 2.755920] i2c /dev entries driver
[ 2.761077] Driver for 1-wire Dallas network protocol.
[ 2.771850] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 2.780364] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 699977 KHz
[ 2.788116] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 700000 KHz
[ 2.797668] sdhci: Secure Digital Host Controller Interface driver
[ 2.803894] sdhci: Copyright(c) Pierre Ossman
[ 2.809936] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.817169] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.825988] omap-aes 4b501000.aes: OMAP AES hw accel rev: 3.2
[ 2.831909] omap-aes 4b501000.aes: will run requests pump with realtime priority
[ 2.839996] omap-aes 4b701000.aes: OMAP AES hw accel rev: 3.2
[ 2.845886] omap-aes 4b701000.aes: will run requests pump with realtime priority
[ 2.853820] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 2.859680] omap-des 480a5000.des: will run requests pump with realtime priority
[ 2.868072] omap-sham 4b100000.sham: hw accel on OMAP rev 4.3
[ 2.875305] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.881103] usbcore: registered new interface driver usbhid
[ 2.886688] usbhid: USB HID core driver
[ 2.892761] wireguard: WireGuard 0.0.20181218 loaded. See www.wireguard.com for information.
[ 2.901367] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld <Jason@zx2c4.com>. All Rights Reserved.
[ 2.911590] NET: Registered protocol family 10
[ 2.916839] Segment Routing with IPv6
[ 2.920593] mip6: Mobile IPv6
[ 2.923583] NET: Registered protocol family 17
[ 2.928131] Key type dns_resolver registered
[ 2.932434] mpls_gso: MPLS GSO support
[ 2.936370] twl: not initialized
[ 2.939605] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.947662] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.955749] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.963806] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.971862] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.979888] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.988281] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1410000 Vs max 1316660
[ 2.996582] omap2_set_init_voltage: unable to find boot up OPP for vdd_core
[ 3.003601] omap2_set_init_voltage: unable to set vdd_core
[ 3.009124] omap2_set_init_voltage: unable to find boot up OPP for vdd_iva
[ 3.016052] omap2_set_init_voltage: unable to set vdd_iva
[ 3.022521] Power Management for TI OMAP4+ devices.
[ 3.027404] OMAP4 PM: u-boot >= v2012.07 is required for full PM support
[ 3.034301] ThumbEE CPU extension supported.
[ 3.034301] Registering SWP/SWPB emulation handler
[ 3.043609] SmartReflex Class3 initialized
[ 3.048278] registered taskstats version 1
[ 3.052490] usb 1-1: new high-speed USB device number 2 using ehci-omap
[ 3.059234] zswap: loaded using pool lzo/zbud
[ 3.065612] Btrfs loaded, crc32c=crc32c-generic
[ 3.070220] AppArmor: AppArmor sha1 policy hashing enabled
[ 3.075805] ima: No TPM chip found, activating TPM-bypass! (rc=-19)
[ 3.075836] ima: Allocated hash algorithm: sha256
[ 3.098236] dmm 4e000000.dmm: initialized all PAT entries
[ 3.105743] Skipping twl internal clock init and using bootloader value (unknown osc rate)
[ 3.141418] twl 0-0048: PIH (irq 149) nested IRQs
[ 3.147338] twl_rtc 48070000.i2c:twl@48:rtc: Power up reset detected.
[ 3.154541] twl_rtc 48070000.i2c:twl@48:rtc: Enabling TWL-RTC
[ 3.163055] twl_rtc 48070000.i2c:twl@48:rtc: rtc core: registered 48070000.i2c:twl@48:rtc as rtc0
[ 3.184234] twl6030_usb 48070000.i2c:twl@48:usb-comparator: Initialized TWL6030 USB module
[ 3.197845] omap_i2c 48070000.i2c: bus 0 rev0.11 at 400 kHz
[ 3.204559] omap_i2c 48072000.i2c: bus 1 rev0.11 at 400 kHz
[ 3.211090] omap_i2c 48060000.i2c: bus 2 rev0.11 at 100 kHz
[ 3.217651] omap_i2c 48350000.i2c: bus 3 rev0.11 at 400 kHz
[ 3.279388] usb 1-1: New USB device found, idVendor=0424, idProduct=9514
[ 3.286163] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 3.293731] hub 1-1:1.0: USB hub found
[ 3.297729] hub 1-1:1.0: 5 ports detected
[ 3.302978] hw-breakpoint: Failed to enable monitor mode on CPU 0.
[ 3.321105] random: fast init done
[ 3.353881] hw-breakpoint: CPU 0 failed to disable vector catch
[ 3.463317] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.463317] [drm] No driver support for vblank timestamp query.
[ 3.479736] omap_hsmmc 480d5000.mmc: card claims to support voltages below defined range
[ 3.499145] mmc1: new SDIO card at address 0001
[ 3.503906] [drm] Cannot find any crtc or sizes
[ 3.509185] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[ 3.518310] twl_rtc 48070000.i2c:twl@48:rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 3.527893] sr_init: No PMIC hook to init smartreflex
[ 3.532989] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 3.541168] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 3.543853] mmc0: host does not support reading read-only switch, assuming write-enable
[ 3.549072] smartreflex smartreflex.2: omap_sr_probe: SmartReflex driver initialized
[ 3.561431] mmc0: new high speed SDHC card at address aaaa
[ 3.564941] of_cfs_init
[ 3.570892] mmcblk0: mmc0:aaaa SM32G 29.7 GiB
[ 3.572814] of_cfs_init: OK
[ 3.580993] vwl1271: disabling
[ 3.582794] mmcblk0: p1
[ 3.588867] VDAC: disabling
[ 3.592163] VANA: disabling
[ 3.595458] VUSB: disabling
[ 3.603240] EXT4-fs (mmcblk0p1): INFO: recovery required on readonly filesystem
[ 3.610961] EXT4-fs (mmcblk0p1): write access will be enabled during recovery
[ 3.630645] usb 1-1.1: new high-speed USB device number 3 using ehci-omap
[ 3.781097] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 3.788085] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 4.161071] EXT4-fs (mmcblk0p1): recovery complete
[ 4.174835] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null)
[ 4.183044] VFS: Mounted root (ext4 filesystem) readonly on device 179:1.
[ 4.193084] devtmpfs: mounted
[ 4.201324] Freeing unused kernel memory: 1024K
[ 4.571228] systemd[1]: System time before build time, advancing clock.
[ 4.578124] [drm] Cannot find any crtc or sizes
[ 4.621337] systemd[1]: systemd 237 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
[ 4.642791] systemd[1]: Detected architecture arm.
Welcome to Ubuntu 18.04.1 LTS!
[ 4.693481] systemd[1]: Set hostname to <arm>.
[ 4.980102] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[ 4.997283] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[ 5.202026] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.203643] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 5.240783] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.248168] systemd[1]: Created slice system-netplan\x2dwpa.slice.
[ OK ] Created slice system-netplan\x2dwpa.slice.
[ 5.281005] random: systemd: uninitialized urandom read (16 bytes read)
[ 5.287994] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 5.321044] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 5.354614] systemd[1]: Starting Set the console keyboard layout...
Starting Set the console keyboard layout...
Starting Load Kernel Modules...
[ OK ] Listening on udev Kernel Socket.
Mounting POSIX Message Queue File System...
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Set up automount Arbitrary Executab…rmats File System Automount Point.
[ OK ] Listening on fsck to fsckd communication Socket.
Starting File System Check on Root Device...
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
Mounting Kernel Debug File System...
[ OK ] Reached target Remote File Systems.
[ OK ] Listening on Journal Audit Socket.
Starting Journal Service...
[ OK ] Reached target Local Encrypted Volumes.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Reached target Paths.
[ OK ] Reached target Swap.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice User and Session Slice.
[ OK ] Reached target Slices.
Starting Create Static Device Nodes in /dev...
Starting udev Coldplug all Devices...
[ OK ] Started Journal Service.
[ OK ] Started Set the console keyboard layout.
[ OK ] Started Load Kernel Modules.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Started File System Check on Root Device.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Started File System Check Daemon to report status.
Starting Remount Root and Kernel File Systems...
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...[ 6.396179] EXT4-fs (mmcblk0p1): re-mounted. Opts: errors=remount-ro
Starting Apply Kernel Variables...
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Apply Kernel Variables.
[ OK ] Reached target Local File Systems (Pre).
Starting udev Kernel Device Manager...
Starting Flush Journal to Persistent Storage...
[ OK ] Reached target Local File Systems.
Starting Set console font and keymap...
Starting Raise network interfaces...
Starting Load/Save Random Seed...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Started Set console font and keymap.
[ OK ] Started Load/Save Random Seed.
Starting Network Service...
[ OK ] Started Network Service.
[ OK ] Started Flush Journal to Persistent Storage.
Starting Create Volatile Files and Directories...
[ OK ] Started Raise network interfaces.
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Started Message of the Day.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Regular background program processing daemon.
Starting Login Service...
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Login Service.
Starting oFono Mobile telephony stack...
Starting Connection service...
Starting Generic Board Startup...
Starting Dispatcher daemon for systemd-networkd...
Starting System Logging Service...
Starting WPA supplicant...
Starting LSB: Start busybox udhcpd at boot time...
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Set the CPU Frequency Scaling governor.
Starting LSB: Load kernel modules needed to enable cpufreq scaling...
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Discard unused blocks once a week.
[ OK ] Started Daily apt download activities.
[ OK ] Started Daily apt upgrade and clean activities.
[ OK ] Reached target Timers.
[ OK ] Found device /dev/ttyS2.
[ OK ] Started System Logging Service.
[ OK ] Started oFono Mobile telephony stack.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started WPA supplicant.
[ OK ] Started Connection service.
[ OK ] Started Generic Board Startup.
Starting Hostname Service...
[ OK ] Started LSB: Start busybox udhcpd at boot time.
[ OK ] Started LSB: Load kernel modules needed to enable cpufreq scaling.
Starting LSB: set CPUFreq kernel parameters...
[ OK ] Started Hostname Service.
[ OK ] Started LSB: set CPUFreq kernel parameters.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Started Dispatcher daemon for systemd-networkd.
[ TIME ] Timed out waiting for device sys-subsystem-net-devices-wlan0.device.
[DEPEND] Dependency failed for WPA supplicant for netplan wlan0.
[ OK ] Reached target Network.
Starting Permit User Sessions...
Starting A high performance web server and a reverse proxy server...
Starting OpenBSD Secure Shell server...
[ OK ] Started Permit User Sessions.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Started Set console scheme.
[ OK ] Created slice system-getty.slice.
[ OK ] Started Getty on tty1.
[ OK Reached target Login Prompts.
[ OK ] Started OpenBSD Secure Shell server.
[ OK ] Started A high performance web server and a reverse proxy server.
[ OK ] Reached target Multi-User System.
[ OK ] Reached target Graphical Interface.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
Ubuntu 18.04.1 LTS arm ttyS2
default username:password is [ubuntu:temppwd]
arm login: ubuntu
Password:
Last login: Sun Jan 28 15:59:57 UTC 2018 on ttyS2
ubuntu@arm:~$ lsmod
Module Size Used by
ubuntu@arm:~$
Didn’t found module that you mentioned. Also lsmod shows empty list.
@marverix, please run “sudo depmod -a” we use compressed modules and it looks like your development pc didn’t generate that… (ubuntu finally updated kmod in 18.10 to support xz modules by default.)
Regards,
Should I get any output? Because sudo depmod -a shows nothing.
Br,
Marek
@marverix, it doesn’t output any information, lsmod should show a few modules loaded, otherwise after a reboot more things should be shown with lsmod…
Regards,
@RobertCNelson you are the Life Saver! After reboot worked like a charm! Thank you so much! 
@RobertCNelson Could you help me also with WiFi? Ethernet is working fine (thru netplan), but WiFi is soft blocked by some reason by kernel (rfkill shows it). I tried to unlock it, but it’s going down all the time… 
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.91-armv7-x14 (marverix@blackstorm) (gcc version 7.3.1 20180425 [linaro-7.3-2018.05 revision d29120a424ecfbc167ef90065c0eeb7f91977701] (Linaro GCC 7.3-2018.05)) #1 SMP PREEMPT Thu Jan 17 17:28:24 CET 2019
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=50c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI OMAP4 PandaBoard-ES
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0xbc800000
[ 0.000000] OMAP4: Map 0xbfe00000 to fe600000 for dram barrier
[ 0.000000] On node 0 totalpages: 261632
[ 0.000000] free_area_init_node: node 0, pgdat c1346e00, node_mem_map ef6f9000
[ 0.000000] Normal zone: 1728 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 196608 pages, LIFO batch:31
[ 0.000000] HighMem zone: 65024 pages, LIFO batch:15
[ 0.000000] OMAP4460 ES1.1
[ 0.000000] random: get_random_bytes called from start_kernel+0x8d/0x37a with crng_init=0
[ 0.000000] percpu: Embedded 18 pages/cpu @ef698000 s41164 r8192 d24372 u73728
[ 0.000000] pcpu-alloc: s41164 r8192 d24372 u73728 alloc=18*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259904
[ 0.000000] Kernel command line: console=ttyO2,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 967468K/1046528K available (10240K kernel code, 1555K rwdata, 4980K rodata, 1024K init, 380K bss, 29908K reserved, 49152K cma-reserved, 210944K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf800000 - 0xbfe00000 ( 6 MB)
.text : 0xc0008000 - 0xc0b00000 (11232 kB)
.init : 0xc1100000 - 0xc1200000 (1024 kB)
.data : 0xc1200000 - 0xc1384f38 (1556 kB)
.bss : 0xc138f654 - 0xc13ee710 ( 381 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] ftrace: allocating 44739 entries in 88 pages
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: CPU: 0 PID: 0 at arch/arm/kernel/insn.c:15 __arm_gen_branch+0x7f/0x84
[ 0.000000] Modules linked in:
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 4.14.91-armv7-x14 #1
[ 0.000000] Hardware name: Generic OMAP4 (Flattened Device Tree)
[ 0.000000] [<c010e539>] (unwind_backtrace) from [<c010a609>] (show_stack+0x11/0x14)
[ 0.000000] [<c010a609>] (show_stack) from [<c09f1101>] (dump_stack+0x5d/0x6c)
[ 0.000000] [<c09f1101>] (dump_stack) from [<c0133da3>] (__warn+0xaf/0xc0)
[ 0.000000] [<c0133da3>] (__warn) from [<c0133e65>] (warn_slowpath_null+0x19/0x1c)
[ 0.000000] [<c0133e65>] (warn_slowpath_null) from [<c010da6f>] (__arm_gen_branch+0x7f/0x84)
[ 0.000000] [<c010da6f>] (__arm_gen_branch) from [<c010d9db>] (ftrace_make_nop+0xf/0x24)
[ 0.000000] [<c010d9db>] (ftrace_make_nop) from [<c01c9fd3>] (ftrace_process_locs+0x227/0x2f0)
[ 0.000000] [<c01c9fd3>] (ftrace_process_locs) from [<c1115b3b>] (ftrace_init+0x6b/0xa8)
[ 0.000000] [<c1115b3b>] (ftrace_init) from [<c1100975>] (start_kernel+0x1d7/0x37a)
[ 0.000000] [<c1100975>] (start_kernel) from [<8000807f>] (0x8000807f)
[ 0.000000] ---[ end trace 566d496eef74c670 ]---
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: CPU: 0 PID: 0 at kernel/trace/ftrace.c:2094 ftrace_bug+0x209/0x29c
[ 0.000000] Modules linked in:
[ 0.000000] CPU: 0 PID: 0 Comm: swapper Tainted: G W 4.14.91-armv7-x14 #1
[ 0.000000] Hardware name: Generic OMAP4 (Flattened Device Tree)
[ 0.000000] [<c010e539>] (unwind_backtrace) from [<c010a609>] (show_stack+0x11/0x14)
[ 0.000000] [<c010a609>] (show_stack) from [<c09f1101>] (dump_stack+0x5d/0x6c)
[ 0.000000] [<c09f1101>] (dump_stack) from [<c0133da3>] (__warn+0xaf/0xc0)
[ 0.000000] [<c0133da3>] (__warn) from [<c0133e65>] (warn_slowpath_null+0x19/0x1c)
[ 0.000000] [<c0133e65>] (warn_slowpath_null) from [<c01c9d19>] (ftrace_bug+0x209/0x29c)
[ 0.000000] [<c01c9d19>] (ftrace_bug) from [<c01c9fe5>] (ftrace_process_locs+0x239/0x2f0)
[ 0.000000] [<c01c9fe5>] (ftrace_process_locs) from [<c1115b3b>] (ftrace_init+0x6b/0xa8)
[ 0.000000] [<c1115b3b>] (ftrace_init) from [<c1100975>] (start_kernel+0x1d7/0x37a)
[ 0.000000] [<c1100975>] (start_kernel) from [<8000807f>] (0x8000807f)
[ 0.000000] ---[ end trace 566d496eef74c671 ]---
[ 0.000000] ftrace failed to modify
[ 0.000000] [<c110da48>] omap_vp_init+0x8/0x13e
[ 0.000000] actual: 67:f0:ba:e9
[ 0.000000] Initializing ftrace call sites
[ 0.000000] ftrace record flags: 0
[ 0.000000] (0)
expected tramp: c010d801
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=2.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] L2C: platform modifies aux control register: 0x0e070000 -> 0x3e470000
[ 0.000000] L2C: DT/platform modifies aux control register: 0x0e070000 -> 0x3e470000
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] OMAP L2C310: ROM does not support power control setting
[ 0.000000] L2C-310 dynamic clock gating disabled, standby mode disabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x4e470000
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node dss_fck
[ 0.000000] OMAP clockevent source: timer1 at 32768 Hz
[ 0.000000] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[ 0.000000] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.002136] Console: colour dummy device 80x30
[ 0.002136] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.002166] This ensures that you still see kernel messages. Please
[ 0.002166] update your kernel commandline.
[ 0.002197] Calibrating delay loop... 1397.55 BogoMIPS (lpj=6987776)
[ 0.087738] pid_max: default: 32768 minimum: 301
[ 0.088043] Security Framework initialized
[ 0.088043] Yama: becoming mindful.
[ 0.088104] AppArmor: AppArmor initialized
[ 0.088195] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.088226] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.089050] CPU: Testing write buffer coherency: ok
[ 0.089080] CPU0: Spectre v2: using BPIALL workaround
[ 0.089355] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.089355] smp: CPU1 parked within kernel, needs reset (0x0 0x80127055)
[ 0.127777] Setting up static identity map for 0x80100000 - 0x80100054
[ 0.147735] Hierarchical SRCU implementation.
[ 0.171997] EFI services will not be available.
[ 0.187713] smp: Bringing up secondary CPUs ...
[ 0.297729] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.297729] CPU1: Spectre v2: using BPIALL workaround
[ 0.297912] smp: Brought up 1 node, 2 CPUs
[ 0.297912] SMP: Total of 2 processors activated (2795.11 BogoMIPS).
[ 0.297943] CPU: All CPU(s) started in SVC mode.
[ 0.299041] devtmpfs: initialized
[ 0.319152] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.319488] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.319519] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.323669] xor: measuring software checksum speed
[ 0.417694] arm4regs : 1010.800 MB/sec
[ 0.517700] 8regs : 792.800 MB/sec
[ 0.617706] 32regs : 764.400 MB/sec
[ 0.717712] neon : 731.600 MB/sec
[ 0.717712] xor: using function: arm4regs (1010.800 MB/sec)
[ 0.717742] pinctrl core: initialized pinctrl subsystem
[ 0.718353] DMI not present or invalid.
[ 0.718719] NET: Registered protocol family 16
[ 0.721710] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.724395] omap_hwmod: l3_main_3 using broken dt data from ocp
[ 0.726837] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.848632] cpuidle: using governor menu
[ 0.856994] OMAP GPIO hardware version 0.1
[ 0.861724] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.861755] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.882049] No ATAGs?
[ 0.882141] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.882171] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.883270] OMAP DMA hardware revision 0.0
[ 0.899475] raid6: using algorithm neonx8 gen() 0 MB/s
[ 0.899475] raid6: .... xor() 0 MB/s, rmw enabled
[ 0.899505] raid6: using neon recovery algorithm
[ 0.912414] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.997924] reg-fixed-voltage wl12xx_vmmc: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_wl12xx_gpio, deferring probe
[ 1.002655] omap-iommu 4a066000.mmu: 4a066000.mmu registered
[ 1.002929] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 1.005279] SCSI subsystem initialized
[ 1.005493] libata version 3.00 loaded.
[ 1.005706] usbcore: registered new interface driver usbfs
[ 1.005767] usbcore: registered new interface driver hub
[ 1.005859] usbcore: registered new device driver usb
[ 1.007232] omap_i2c 48070000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c1_pins, deferring probe
[ 1.007263] omap_i2c 48072000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c2_pins, deferring probe
[ 1.007324] omap_i2c 48060000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c3_pins, deferring probe
[ 1.007354] omap_i2c 48350000.i2c: could not find pctldev for node /ocp/l4@4a000000/scm@100000/pinmux@40/pinmux_i2c4_pins, deferring probe
[ 1.007568] media: Linux media interface: v0.10
[ 1.007629] Linux video capture interface: v2.00
[ 1.007781] pps_core: LinuxPPS API ver. 1 registered
[ 1.007781] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 1.007812] PTP clock support registered
[ 1.007934] dmi: Firmware registration failed.
[ 1.008453] omap-mailbox 4a0f4000.mailbox: omap mailbox rev 0x400
[ 1.009887] NetLabel: Initializing
[ 1.009918] NetLabel: domain hash size = 128
[ 1.009918] NetLabel: protocols = UNLABELED CIPSOv4 CALIPSO
[ 1.009979] NetLabel: unlabeled traffic allowed by default
[ 1.010559] clocksource: Switched to clocksource 32k_counter
[ 1.141540] VFS: Disk quotas dquot_6.6.0
[ 1.141632] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.142242] AppArmor: AppArmor Filesystem Enabled
[ 1.155181] NET: Registered protocol family 2
[ 1.155853] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 1.155944] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 1.156066] TCP: Hash tables configured (established 8192 bind 8192)
[ 1.156219] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 1.156280] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 1.156524] NET: Registered protocol family 1
[ 1.167205] RPC: Registered named UNIX socket transport module.
[ 1.167236] RPC: Registered udp transport module.
[ 1.167236] RPC: Registered tcp transport module.
[ 1.167236] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.170379] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 1.170684] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 1.173950] audit: initializing netlink subsys (disabled)
[ 1.174163] audit: type=2000 audit(1.160:1): state=initialized audit_enabled=0 res=1
[ 1.175018] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 1.180938] zbud: loaded
[ 1.193939] NFS: Registering the id_resolver key type
[ 1.193969] Key type id_resolver registered
[ 1.194000] Key type id_legacy registered
[ 1.194000] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.194213] fuse init (API version 7.26)
[ 1.198852] jitterentropy: Initialization failed with host not compliant with requirements: 2
[ 1.198974] Key type asymmetric registered
[ 1.198974] Asymmetric key parser 'x509' registered
[ 1.199066] bounce: pool size: 64 pages
[ 1.199127] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 1.199279] io scheduler noop registered
[ 1.199310] io scheduler deadline registered
[ 1.199493] io scheduler cfq registered (default)
[ 1.199493] io scheduler mq-deadline registered
[ 1.204498] pinctrl-single 4a100040.pinmux: 203 pins at pa fc100040 size 406
[ 1.205047] pinctrl-single 4a31e040.pinmux: 28 pins at pa fc31e040 size 56
[ 1.220977] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled
[ 1.223602] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 32, base_baud = 3000000) is a 8250
[ 1.224334] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 33, base_baud = 3000000) is a 8250
[ 1.225036] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 34, base_baud = 3000000) is a 8250
[ 2.453948] console [ttyS2] enabled
[ 2.458190] 4806e000.serial: ttyS3 at MMIO 0x4806e000 (irq = 35, base_baud = 3000000) is a 8250
[ 2.470825] omapdss_dss 58000000.dss: 58000000.dss supply vdda_video not found, using dummy regulator
[ 2.480194] DSS: OMAP DSS rev 4.0
[ 2.486358] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 2.494445] OF: graph: no port node found in /ocp/dss@58000000/encoder@58005000
[ 2.501892] omapdss_dss 58000000.dss: bound 58005000.encoder (ops dsi_component_ops)
[ 2.510345] omapdss_dss 58000000.dss: bound 58006000.encoder (ops hdmi4_component_ops)
[ 2.520385] connector-dvi connector0: failed to parse ddc-i2c-bus
[ 2.529022] Error: Driver 'tfp410' is already registered, aborting...
[ 2.541229] usbcore: registered new interface driver dln2
[ 2.552246] libphy: Fixed MDIO Bus: probed
[ 2.561798] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.568389] ehci-platform: EHCI generic platform driver
[ 2.573974] ehci-omap: OMAP-EHCI Host Controller driver
[ 2.599609] ehci-omap 4a064c00.ehci: EHCI Host Controller
[ 2.605102] ehci-omap 4a064c00.ehci: new USB bus registered, assigned bus number 1
[ 2.612945] ehci-omap 4a064c00.ehci: irq 142, io mem 0x4a064c00
[ 2.640594] ehci-omap 4a064c00.ehci: USB 2.0 started, EHCI 1.00
[ 2.646789] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.653656] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.660919] usb usb1: Product: EHCI Host Controller
[ 2.665832] usb usb1: Manufacturer: Linux 4.14.91-armv7-x14 ehci_hcd
[ 2.672241] usb usb1: SerialNumber: 4a064c00.ehci
[ 2.677581] hub 1-0:1.0: USB hub found
[ 2.681427] hub 1-0:1.0: 3 ports detected
[ 2.686889] usbcore: registered new interface driver usb-storage
[ 2.693969] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 2.699737] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 2.707855] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.714691] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.721984] usb usb2: Product: MUSB HDRC host driver
[ 2.726989] usb usb2: Manufacturer: Linux 4.14.91-armv7-x14 musb-hcd
[ 2.733398] usb usb2: SerialNumber: musb-hdrc.1.auto
[ 2.738922] hub 2-0:1.0: USB hub found
[ 2.742767] hub 2-0:1.0: 1 port detected
[ 2.755920] i2c /dev entries driver
[ 2.761077] Driver for 1-wire Dallas network protocol.
[ 2.771881] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 2.780364] cpufreq: cpufreq_online: CPU0: Running at unlisted freq: 699977 KHz
[ 2.788146] cpufreq: cpufreq_online: CPU0: Unlisted initial frequency changed to: 700000 KHz
[ 2.797668] sdhci: Secure Digital Host Controller Interface driver
[ 2.803894] sdhci: Copyright(c) Pierre Ossman
[ 2.809936] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.817169] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.826019] omap-aes 4b501000.aes: OMAP AES hw accel rev: 3.2
[ 2.831939] omap-aes 4b501000.aes: will run requests pump with realtime priority
[ 2.840026] omap-aes 4b701000.aes: OMAP AES hw accel rev: 3.2
[ 2.845916] omap-aes 4b701000.aes: will run requests pump with realtime priority
[ 2.853851] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 2.859741] omap-des 480a5000.des: will run requests pump with realtime priority
[ 2.868133] omap-sham 4b100000.sham: hw accel on OMAP rev 4.3
[ 2.875335] hidraw: raw HID events driver (C) Jiri Kosina
[ 2.881103] usbcore: registered new interface driver usbhid
[ 2.886718] usbhid: USB HID core driver
[ 2.892791] wireguard: WireGuard 0.0.20181218 loaded. See www.wireguard.com for information.
[ 2.901397] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld <Jason@zx2c4.com>. All Rights Reserved.
[ 2.911651] NET: Registered protocol family 10
[ 2.916900] Segment Routing with IPv6
[ 2.920654] mip6: Mobile IPv6
[ 2.923614] NET: Registered protocol family 17
[ 2.928161] Key type dns_resolver registered
[ 2.932464] mpls_gso: MPLS GSO support
[ 2.936401] twl: not initialized
[ 2.939636] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.947692] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.955780] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.963836] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.971893] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.979919] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1375000 Vs max 1316660
[ 2.988220] twl6030_uv_to_vsel:OUT OF RANGE! non mapped vsel for 1410000 Vs max 1316660
[ 2.996520] omap2_set_init_voltage: unable to find boot up OPP for vdd_core
[ 3.003540] omap2_set_init_voltage: unable to set vdd_core
[ 3.009063] omap2_set_init_voltage: unable to find boot up OPP for vdd_iva
[ 3.015960] omap2_set_init_voltage: unable to set vdd_iva
[ 3.022460] Power Management for TI OMAP4+ devices.
[ 3.027343] OMAP4 PM: u-boot >= v2012.07 is required for full PM support
[ 3.034423] ThumbEE CPU extension supported.
[ 3.034423] Registering SWP/SWPB emulation handler
[ 3.043548] SmartReflex Class3 initialized
[ 3.048278] registered taskstats version 1
[ 3.052429] usb 1-1: new high-speed USB device number 2 using ehci-omap
[ 3.059234] zswap: loaded using pool lzo/zbud
[ 3.065582] Btrfs loaded, crc32c=crc32c-generic
[ 3.070190] AppArmor: AppArmor sha1 policy hashing enabled
[ 3.070190] ima: No TPM chip found, activating TPM-bypass! (rc=-19)
[ 3.082061] ima: Allocated hash algorithm: sha256
[ 3.097839] dmm 4e000000.dmm: initialized all PAT entries
[ 3.105224] Skipping twl internal clock init and using bootloader value (unknown osc rate)
[ 3.131286] hw-breakpoint: Failed to enable monitor mode on CPU 0.
[ 3.137573] twl 0-0048: PIH (irq 149) nested IRQs
[ 3.143829] hw-breakpoint: CPU 0 failed to disable vector catch
[ 3.152008] twl_rtc 48070000.i2c:twl@48:rtc: Enabling TWL-RTC
[ 3.160400] twl_rtc 48070000.i2c:twl@48:rtc: rtc core: registered 48070000.i2c:twl@48:rtc as rtc0
[ 3.181610] twl6030_usb 48070000.i2c:twl@48:usb-comparator: Initialized TWL6030 USB module
[ 3.195617] omap_i2c 48070000.i2c: bus 0 rev0.11 at 400 kHz
[ 3.201690] omap_i2c 48072000.i2c: bus 1 rev0.11 at 400 kHz
[ 3.208007] omap_i2c 48060000.i2c: bus 2 rev0.11 at 100 kHz
[ 3.214569] omap_i2c 48350000.i2c: bus 3 rev0.11 at 400 kHz
[ 3.262115] usb 1-1: New USB device found, idVendor=0424, idProduct=9514
[ 3.268890] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 3.276702] hub 1-1:1.0: USB hub found
[ 3.280548] hub 1-1:1.0: 5 ports detected
[ 3.290283] random: fast init done
[ 3.433319] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 3.440002] [drm] No driver support for vblank timestamp query.
[ 3.450592] omap_hsmmc 480d5000.mmc: card claims to support voltages below defined range
[ 3.470489] mmc1: new SDIO card at address 0001
[ 3.475219] [drm] Cannot find any crtc or sizes
[ 3.480743] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
[ 3.490905] twl_rtc 48070000.i2c:twl@48:rtc: setting system clock to 2019-01-18 18:09:21 UTC (1547834961)
[ 3.491882] sr_init: No PMIC hook to init smartreflex
[ 3.505798] smartreflex smartreflex.0: omap_sr_probe: SmartReflex driver initialized
[ 3.513732] smartreflex smartreflex.1: omap_sr_probe: SmartReflex driver initialized
[ 3.521789] smartreflex smartreflex.2: omap_sr_probe: SmartReflex driver initialized
[ 3.529754] of_cfs_init
[ 3.532257] of_cfs_init: OK
[ 3.536163] vwl1271: disabling
[ 3.541351] VDAC: disabling
[ 3.544616] VANA: disabling
[ 3.547912] VUSB: disabling
[ 3.550750] mmc0: host does not support reading read-only switch, assuming write-enable
[ 3.559295] Waiting for root device /dev/mmcblk0p1...
[ 3.564575] mmc0: new high speed SDHC card at address aaaa
[ 3.570556] mmcblk0: mmc0:aaaa SM32G 29.7 GiB
[ 3.577972] mmcblk0: p1
[ 3.608734] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null)
[ 3.616882] VFS: Mounted root (ext4 filesystem) readonly on device 179:1.
[ 3.620605] usb 1-1.1: new high-speed USB device number 3 using ehci-omap
[ 3.633850] devtmpfs: mounted
[ 3.642272] Freeing unused kernel memory: 1024K
[ 3.781066] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 3.787994] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 4.182891] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 4.213989] systemd[1]: systemd 237 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
[ 4.236175] systemd[1]: Detected architecture arm.
[ 4.293548] systemd[1]: Set hostname to <arm>.
[ 4.480926] [drm] Cannot find any crtc or sizes
[ 4.599731] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
[ 4.616943] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
[ 4.836456] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.843536] systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.
[ 4.890777] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.890808] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 4.940673] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.947387] systemd[1]: Reached target Remote File Systems.
[ 4.970947] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 5.030670] systemd[1]: Reached target Local Encrypted Volumes.
[ 6.389221] EXT4-fs (mmcblk0p1): re-mounted. Opts: errors=remount-ro
[ 6.735168] systemd-journald[146]: Received request to flush runtime journal from PID 1
[ 8.779541] Bluetooth: Core ver 2.22
[ 8.779663] NET: Registered protocol family 31
[ 8.779693] Bluetooth: HCI device and connection manager initialized
[ 8.779693] Bluetooth: HCI socket layer initialized
[ 8.779724] Bluetooth: L2CAP socket layer initialized
[ 8.779754] Bluetooth: SCO socket layer initialized
[ 9.411407] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
[ 10.096160] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58006000.encoder mapping ok
[ 10.096160] omap-hdmi-audio omap-hdmi-audio.0.auto: ASoC: no DMI vendor name!
[ 10.165740] smsc95xx v1.0.6
[ 10.241516] omap-abe-twl6040 sound: twl6040-legacy <-> 40132000.mcpdm mapping ok
[ 10.241516] omap-abe-twl6040 sound: ASoC: no DMI vendor name!
[ 10.305053] smsc95xx 1-1.1:1.0 eth0: register 'smsc95xx' at usb-4a064c00.ehci-1.1, smsc95xx USB 2.0 Ethernet, 02:02:01:9a:1b:a0
[ 10.305236] usbcore: registered new interface driver smsc95xx
[ 10.416076] smsc95xx 1-1.1:1.0 eth0: hardware isn't capable of remote wakeup
[ 10.416320] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 11.294494] wlcore: WARNING Detected unconfigured mac address in nvs, derive from fuse instead.
[ 11.294494] wlcore: WARNING Your device performance is not optimized.
[ 11.295593] wlcore: WARNING Please use the calibrator tool to configure your device.
[ 11.299255] wlcore: loaded
[ 11.914886] wlcore: firmware booted (Rev 6.3.10.0.142)
[ 11.927764] smsc95xx 1-1.1:1.0 eth0: link up, 100Mbps, full-duplex, lpa 0xC5E1
[ 11.935455] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 11.952239] wlcore: down
[ 11.955352] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 12.040618] 8021q: 802.1Q VLAN Support v1.8
[ 174.432830] wlcore: firmware booted (Rev 6.3.10.0.142)
[ 174.447692] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Br,
@marverix, while at work i can’t really test 2.4Ghz as our routers block rogue access points… connman is able to disable the rfkill lock…
ubuntu@arm:~$ journalctl | grep wlan0
Jan 18 19:55:22 arm connmand[261]: wlan0 {create} index 3 type 1 <ETHER>
Jan 18 19:55:22 arm connmand[261]: wlan0 {update} flags 4098 <DOWN>
Jan 18 19:55:22 arm connmand[261]: wlan0 {newlink} index 3 address 1C:45:93:5C:F7:79 mtu 1500
Jan 18 19:55:22 arm connmand[261]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 18 19:55:22 arm connmand[261]: Adding interface wlan0 [ wifi ]
Jan 18 20:20:39 arm kernel: IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Jan 18 20:20:39 arm connmand[261]: wlan0 {update} flags 36931 <UP,RUNNING>
Jan 18 20:20:39 arm connmand[261]: wlan0 {newlink} index 3 address 1C:45:93:5C:F7:79 mtu 1500
Jan 18 20:20:39 arm connmand[261]: wlan0 {newlink} index 3 operstate 0 <UNKNOWN>
Jan 18 20:20:39 arm connmand[261]: wlan0 {update} flags 36867 <UP>
Jan 18 20:20:39 arm connmand[261]: wlan0 {newlink} index 3 address 1C:45:93:5C:F7:79 mtu 1500
Jan 18 20:20:39 arm connmand[261]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 18 20:20:39 arm connmand[261]: wlan0 {newlink} index 3 address 1C:45:93:5C:F7:79 mtu 1500
Jan 18 20:20:39 arm connmand[261]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 18 20:20:39 arm wpa_supplicant[260]: nl80211: Could not set interface 'p2p-dev-wlan0' UP
Jan 18 20:20:39 arm wpa_supplicant[260]: nl80211: deinit ifname=p2p-dev-wlan0 disabled_11b_rates=0
Jan 18 20:20:39 arm wpa_supplicant[260]: p2p-dev-wlan0: Failed to initialize driver interface
Jan 18 20:23:06 arm wpa_supplicant[260]: wlan0: SME: Trying to authenticate with 40:4e:36:82:21:3e (SSID='Avenger' freq=2422 MHz)
Jan 18 20:23:06 arm kernel: wlan0: authenticate with 40:4e:36:82:21:3e
Jan 18 20:23:06 arm kernel: wlan0: send auth to 40:4e:36:82:21:3e (try 1/3)
Jan 18 20:23:06 arm kernel: wlan0: send auth to 40:4e:36:82:21:3e (try 2/3)
Jan 18 20:23:06 arm kernel: wlan0: send auth to 40:4e:36:82:21:3e (try 3/3)
Jan 18 20:23:06 arm kernel: wlan0: authentication with 40:4e:36:82:21:3e timed out
ubuntu@arm:~$ uname -r ; cat /proc/device-tree/model
4.19.15-armv7-x19.2
TI OMAP4 PandaBoard-ES
Regards,
ubuntu@arm:~$ journalctl | grep wlan0
Jan 18 18:07:44 arm systemd-networkd[1274]: wlan0: found matching network '/run/systemd/network/10-netplan-wlan0.n etwork', based on potentially unpredictable ifname
Jan 18 18:07:44 arm systemd-networkd[1274]: wlan0: IPv6 successfully enabled
Jan 18 18:07:44 arm systemd-networkd[1274]: wlan0: Could not bring up interface: Operation not possible due to RF- kill
Jan 18 18:09:11 arm wpa_supplicant[316]: nl80211: deinit ifname=p2p-dev-wlan0 disabled_11b_rates=0
Jan 18 18:09:11 arm connmand[314]: Remove interface wlan0 [ wifi ]
Jan 18 18:09:11 arm connmand[314]: wlan0 {remove} index 3
Jan 18 18:09:11 arm wpa_supplicant[316]: nl80211: deinit ifname=wlan0 disabled_11b_rates=0
Jan 18 18:09:29 arm connmand[273]: wlan0 {create} index 3 type 1 <ETHER>
Jan 18 18:09:29 arm connmand[273]: wlan0 {update} flags 4098 <DOWN>
Jan 18 18:09:29 arm connmand[273]: wlan0 {newlink} index 3 address C8:A0:30:75:A3:C9 mtu 1500
Jan 18 18:09:29 arm connmand[273]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 18 18:09:29 arm connmand[273]: Adding interface wlan0 [ wifi ]
Jan 18 18:09:29 arm kernel: IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Jan 18 18:09:29 arm connmand[273]: wlan0 {update} flags 36931 <UP,RUNNING>
Jan 18 18:09:29 arm connmand[273]: wlan0 {newlink} index 3 address C8:A0:30:75:A3:C9 mtu 1500
Jan 18 18:09:29 arm connmand[273]: wlan0 {newlink} index 3 operstate 0 <UNKNOWN>
Jan 18 18:09:29 arm connmand[273]: wlan0 {update} flags 36866 <DOWN>
Jan 18 18:09:29 arm connmand[273]: wlan0 {newlink} index 3 address C8:A0:30:75:A3:C9 mtu 1500
Jan 18 18:09:29 arm connmand[273]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 18 18:09:30 arm systemd-networkd[184]: wlan0: found matching network '/run/systemd/network/10-netplan-wlan0.ne twork', based on potentially unpredictable ifname
Jan 18 18:09:30 arm systemd-networkd[184]: wlan0: IPv6 successfully enabled
Jan 18 18:09:30 arm systemd-networkd[184]: wlan0: Could not bring up interface: Operation not possible due to RF-k ill
Jan 18 18:09:30 arm systemd[1]: Found device /sys/subsystem/net/devices/wlan0.
Jan 18 18:09:30 arm systemd[1]: Started WPA supplicant for netplan wlan0.
Jan 18 18:09:30 arm wpa_supplicant[467]: Delete '/run/wpa_supplicant/wlan0' manually if it is not used anymore
Jan 18 18:09:30 arm wpa_supplicant[467]: nl80211: deinit ifname=wlan0 disabled_11b_rates=0
Jan 18 18:09:30 arm systemd[1]: netplan-wpa@wlan0.service: Main process exited, code=exited, status=255/n/a
Jan 18 18:09:30 arm systemd[1]: netplan-wpa@wlan0.service: Failed with result 'exit-code'.
Jan 18 18:10:56 arm sudo[521]: ubuntu : TTY=ttyO2 ; PWD=/home/ubuntu ; USER=root ; COMMAND=/sbin/ifconfig wlan0 up
Jan 18 18:12:12 arm connmand[273]: wlan0 {update} flags 36867 <UP>
Jan 18 18:12:12 arm connmand[273]: wlan0 {newlink} index 3 address C8:A0:30:75:A3:C9 mtu 1500
Jan 18 18:12:12 arm connmand[273]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 18 18:12:12 arm kernel: IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Jan 18 18:12:20 arm sudo[583]: ubuntu : TTY=ttyO2 ; PWD=/home/ubuntu ; USER=root ; COMMAND=/sbin/ifconfig wlan0 up
Jan 18 19:49:56 arm wpa_supplicant[285]: nl80211: deinit ifname=p2p-dev-wlan0 disabled_11b_rates=0
Jan 18 19:49:56 arm wpa_supplicant[285]: p2p-dev-wlan0: CTRL-EVENT-TERMINATING
Jan 18 19:49:56 arm connmand[273]: Remove interface wlan0 [ wifi ]
Jan 18 19:49:56 arm wpa_supplicant[285]: nl80211: deinit ifname=wlan0 disabled_11b_rates=0
Jan 18 19:49:56 arm connmand[273]: wlan0 {remove} index 3
Jan 18 19:49:56 arm wpa_supplicant[285]: wlan0: CTRL-EVENT-TERMINATING
Jan 19 08:37:03 arm connmand[321]: wlan0 {create} index 3 type 1 <ETHER>
Jan 19 08:37:03 arm connmand[321]: wlan0 {update} flags 4098 <DOWN>
Jan 19 08:37:03 arm connmand[321]: wlan0 {newlink} index 3 address C8:A0:30:75:A3:C9 mtu 1500
Jan 19 08:37:03 arm connmand[321]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 19 08:37:03 arm connmand[321]: Adding interface wlan0 [ wifi ]
Jan 19 08:37:03 arm kernel: IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Jan 19 08:37:03 arm connmand[321]: wlan0 {update} flags 36931 <UP,RUNNING>
Jan 19 08:37:03 arm connmand[321]: wlan0 {newlink} index 3 address C8:A0:30:75:A3:C9 mtu 1500
Jan 19 08:37:03 arm connmand[321]: wlan0 {newlink} index 3 operstate 0 <UNKNOWN>
Jan 19 08:37:03 arm connmand[321]: wlan0 {update} flags 36866 <DOWN>
Jan 19 08:37:03 arm connmand[321]: wlan0 {newlink} index 3 address C8:A0:30:75:A3:C9 mtu 1500
Jan 19 08:37:03 arm connmand[321]: wlan0 {newlink} index 3 operstate 2 <DOWN>
Jan 19 08:37:03 arm systemd-networkd[186]: wlan0: found matching network '/run/systemd/network/10-netplan-wlan0.ne twork', based on potentially unpredictable ifname
Jan 19 08:37:03 arm systemd-networkd[186]: wlan0: IPv6 successfully enabled
Jan 19 08:37:03 arm systemd-networkd[186]: wlan0: Could not bring up interface: Operation not possible due to RF-k ill
Jan 19 08:37:03 arm systemd[1]: Found device /sys/subsystem/net/devices/wlan0.
Jan 19 08:37:03 arm systemd[1]: Started WPA supplicant for netplan wlan0.
Jan 19 08:37:04 arm wpa_supplicant[465]: Delete '/run/wpa_supplicant/wlan0' manually if it is not used anymore
Jan 19 08:37:04 arm wpa_supplicant[465]: nl80211: deinit ifname=wlan0 disabled_11b_rates=0
Jan 19 08:37:04 arm systemd[1]: netplan-wpa@wlan0.service: Main process exited, code=exited, status=255/n/a
Jan 19 08:37:04 arm systemd[1]: netplan-wpa@wlan0.service: Failed with result 'exit-code'.
ubuntu@arm:~$ sudo apt install connmanctl
[sudo] password for ubuntu:
Reading package lists... Done
Building dependency tree
Reading state information... Done
E: Unable to locate package connmanctl
ubuntu@arm:~$ sudo apt install connman
Reading package lists... Done
Building dependency tree
Reading state information... Done
connman is already the newest version (1.36-1rcnee3~bionic+20180517).
0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded.
ubuntu@arm:~$ connmanctl
connmanctl> enable wifi
Enabled wifi
connmanctl> scan wifi
Error /net/connman/technology/wifi: No carrier
connmanctl> services
*AO Wired ethernet_0202019a1ba0_cable
connmanctl> exit
ubuntu@arm:~$
And:
ubuntu@arm:~$ uname -r ; cat /proc/device-tree/model
4.14.91-armv7-x14
TI OMAP4 PandaBoard-ES
I will try tomorrow with new kernel then. Thanks one more time for your time and huge help!
Br,
Marek
@marverix, does this service file fix it?
Regards,
Hello @RobertCNelson,
Nope… Command rfkill unblock wifi is not working for me. I mean in theory it is working, but still for some reason wifi is going down. In free time I will try 4.19 kernel. My last idea is to try to calibrate adapter according to TI tutorial.
Br,
Marek