Hello.I am looking to replace the following part .I have a SOP-8 pin ic chip (width 4.75mm x on pin side length is 5.5mm x thickness 1.18mm) with the following identification on top it’s either DTQ 6604 or DTO 6604 DK370.PCB part number if helpfull is CGT04A-T1-V03 DF-2H E199900 94V-0.It’s a cordless trimmer/edger with a 20 volt Li-ion battery.Any help would be appreciated.Thank you.
Can you provide a close-up photo of the part and another from further out with adjacent parts visible to help try to ID?
In a message dated 2024-10-07 4:27:23 PM Eastern Daylight Time, notifications@digikey.discoursemail.com writes:
On the second photo to your right. the terminals being used are highlighted in white symbols.
Hi triaxon3 ,
Unfortunately am unable to identify this part.