BSP752T
BSP752R
What the difference on these parts? Can’t find the answer on datasheet. help
the only difference between these two parts is that
BSP752TXUMA1 as IC PWR SWITCH N-CHAN 1:1 PDSO-8 from Infineon Technologies is missing one feature vs BSP752RXUMA2 of the same miniPROFET® series including an open load detection in OFF-state with an external resistor.
Hi,
Welcome to the Digikey tech forum. Part BSP752R has the diagnostic feedback option on pin 4, see page 2 on the datasheet. Part BSP752T does not have that feature, see page 2 on the datasheet you will see pin 4 is a no connect. As Rolf also noted this is listed in the features on the first page of the datasheets.