Part Number request. unable to find

Hi there Team!
I hope this finds you all well.

I am looking for Deutsch Connectors, but unable to locate them. the specs are listed below. please advise on an accurate model number that is in stock for purchase.

  • 2x1 and 2x2 contact models
  • IP66 or higher approved
  • Both Male And Female
  • contacts included.

Thank you so much for any assistance! I look forward to hearing from you.

Regards.

What wire gauge are you working with? You’ve got options like 14-16AWG, 20AWG or 16-22AWG

Do you need Gold or Nickle plated contacts?

You also have options for machined contacts like the following, they cost a little more:


Otherwise you have the option of stamped contacts like:

To get you started I would look at the following two and then we have all the associated product including mating connectors linked towards the bottom of the page:
DT06-4S TE Connectivity Deutsch Connectors | Connectors, Interconnects | DigiKey

DT06-2S TE Connectivity Deutsch Connectors | Connectors, Interconnects | DigiKey

@Kristof_2649 WONDERFUL!

This is exactly what i am looking for. you are a life saver.

I do however need to know one thing. i know this doesn’t come with contacts, but does this have both the M and F parts, or do i have to buy them separately?

Thanks Again!

@Kristof_2649 I Found This. looking at it, i am fairly confident this is what i need? (Complete)
Male/Female with Pins and Sockets installed?

Thanks in advance.

These would be sold separately. As an example, if you ordered housing part DT06-2S you would need to order one of the associated socket contacts based on the size wire you will be using. You would also need to order the mating connector, part DT04-2P and the associated pin contacts which again will be based on the wire size and don’t forget the wedgelocks for each housing, part W2S to be used with DT06-2S and part W2P to be used with DT04-2P . In order to complete the set for this example you would order 6 separate part numbers for the housings, crimp contacts and wedges. What I gave is an example of what may work for you and as Kristof mentioned you can search all the associated product including mating connectors and contacts linked towards the bottom of the page:

@Steve_Fellman Thank you! this is very informative. I Think everything is solved at this point now. both you and @Kristof_2649 have been wonderful.

Thanks for all your help!