Hello, I’m in need of replaced some LED boards that are inside my warehouse light fixtures. Any information on obtaining a board that could be custom fit to these specifications would also be useful.
The specifications are as follows:
DC+ 20001 V4.0 Marked: 35 & 50
1166x32x1.0mm
94V-0 HD-1 E346669
The lighting fixtures typically are custom mass produced boards with the markings on them being known to the OEM.
I see, does this mean that I can have these custom made? If so, any recommendations for supplier? These were installed by a third party company who contracted the service for an electrical incentive. If no, I’ll have to speak with the powers at be, about having a company come out to the warehouse.
While custom, they would also need to be ordered in mass quantities that would make having some on hand not be feasible. It would be more cost effective to replace the fixture.