PUI Audio Exciter

This is the place to ask any questions related to the ASX10108-SPD-R (668-1584-ND) exciter speaker from PUI Audio, Inc.. This is very similar to a traditional speaker; however, this turns the surface that it is applied to into a speaker. There is a voice coil that is directly coupled a surface. This excites the surface producing the sound that a traditional speaker would produce. Different surfaces will give different frequency responses. Denser materials allow for more high frequency output. Bendable materials allow for more low and mid-range frequency output.

For the video we used several different surfaces to produce different tonal responses from the exciter.

Video -

image

EEWiki - http://eewiki.net/display/DKSB/PUI+eXciter
Product - ASX10108-SPD-R / 668-1584-ND

Hi there, any recommendations for which amplifier to use with this exciter? I’ve used The PUI ASX03608-R with a Dayton DTA-1 on wooden surfaces such as violins and small percussion instruments. This set-up works very well, but I need more gain power and the ASX10108-SPD-R seems well-suited for this. Thanks a lot in advance!
All best,
Mads

Welcome to the TechForum Madsemildreyer. The most appropriate driver that my product manager recommended was 668-1621-ND for this application.