Question for ADXL354B

I have the ADXL354B without an evaluation board. I understand I can’t use this product without board. What I’d like to know is, can I get just the eval board or do I need to buy the version that comes with the eval board? If I can only get the eval board, how can I connect the accelerometer to it? Thank you.

@Mer123

At this time I only see that we have the eval board that has the chip on it already.
505-EVAL-ADXL354BZ-ND
EVAL-ADXL354BZ Analog Devices Inc. | Development Boards, Kits, Programmers | DigiKey

Also, I am not seeing that the manufacturer lists a version that does not come with a chip pre-installed.

1 Like

This should only be the chip part. When I look at the datasheet in the link I provided, it gives information about the chip. The image in your link shows an evaluation board with a chip, but the datasheet only contains information about the evaluation board. Also, the description says “EVAL BOARD FOR ADXL354B.” This is the part that confuse me. I currently only have the chip part. In the product stands in your link, does it have an eval board with a chip on it, or does it only have an eval board, and am I the one who needs to connect the chip to it? Thank you.

@Mer123

Correct, The 505-ADXL354BEZ-ND would be just the sensor chip.

The 505-EVAL-ADXL354BZ-ND would be an evaluation board that already has a ADXL354B sensor chip installed on the board.

I had not seen that Analog Devices Inc currently lists a version of the 505-EVAL-ADXL354BZ-ND without the chip already installed on the board.

For the 505-ADXL354BEZ-ND sensor chip you already have on hand. If you want it installed on a board you would need to have a board cut to accept it and then solder the chip you have onto the board.