Relay pin positions

I am looking for STDP relays with 12VDC coil that can be mounted on a standard 0.100" grid board. It seems that all the relays I can find (such as this one) have through pins spaced 12.0mm, 12.2mm and 2.2mm apart. Do these fit on any standard board? What I find odd is that I had no trouble finding STSP relays with through-hole pins that fit a 0.100" grid. Can I do the same with STDP? Thanks.

I did some checking on this, take a look at Digikey part number Z221-ND as an option, this has the .1 inch spacing you are looking for, here is the link for quick reference to the part information, https://www.digikey.com/product-detail/en/omron-electronics-inc-emc-div/G5Q-1-DC12/Z221-ND/355239. The G5Q data sheet link will show this relay has the pin spacing you are looking for.

Steve, that’s the ticket! I wonder why it wasn’t coming up in the searches I was doing. Perhaps I simply overlooked it. At any rate, it’s just right. Thanks for your very prompt help.