Replacement for AMD Spartan IC

Hello,

I need help identifying a replacement for an AMD Spartan Xilinx IC with the part number XC6SLX25, FGG484BIV1601, 2C. Have attached a picture of the same. The closest that I can find is XC6SLX25-2FGG484I. However, am not sure whether it will work as a replacement.

Kindly assist.

Yes, both of these parts should work as direct replacement:

484 FBGA

XC6SLX25-2FGG484I with -40°C to +100°C (TJ) Industrial Temperature Range
C6SLX25-2FGG484C with reduced -40°C to +85°C Consumer Temperature grade maximum specification for the Junction

Thank you very much

you’re very welcome – we’re here to support you … :wink: