I purchased three landscape lights not realizing that they are 120v and not 12v. I cannot return the lights and i cannot run 120v to them. I do have low voltage to that location already so I thought the easy solution would be to open them up remove their drivers and connect them to a similar spec driver with 3x more Amps. I noticed that the drivers in the light said “OUTPUT:DC26-42V 300mA” and assumed that as long as I can figure out what volts the led runs on I can just buy a matching power supply and connect the light and power supply using the low voltage wire I already have run there. Well after i removed the drivers, i have come to realize that the solution may not be so simple. Long story short can i do what I have drawn out below. Any input would be appreciated.
All wiring below will be 12 gauge and run in parallel