Does anyone recognize this part. 6W power resistor?
I’m referring to the two white blocks
Hello emilsik36,
Welcome to the DigiKey TechForum.
These are 6W power resistor, and probably a wirewound style.
The J is for 5% tolerance.
I can not read the ohm rating, but it looks like 390, 396 or something similar.
You will have to take a better look from different angles to verify the correct ratings.
If the rating is 390 ohms, the closest we have is 7W, which would be a better resistor.
Click here for A137106-ND.
Please check the datasheet to verify dimensions and compatibility.
Thank you for the reply David!
It does have a 390 ohm rating.
The specs on the part you sent me has a length of 1.417” the two resistors I’m looking to replace are only 1” in length. Any chance you might have something closer in size? Maybe I could make that one work/fit?
I appreciate the help!
Emil