Resistor Type and where to purchase

Hello, I was wondering if anyone would be able to identify these electronic components on this PCB. This is from an outdoor air conditioning unit. Any help is appreciated.

file:///Users/braydenkinkle/Library/Messages/Attachments/85/05/29FADF99-596B-4D9B-BD2B-0E14B57246E3/Resized_20250804_182321.jpeg

file:///Users/braydenkinkle/Library/Messages/Attachments/db/11/8D7BD5B6-1104-4FB9-98B6-EF4A09AF22D1/Resized_20250806_184815.jpeg

@braydenkinkle7

For the last two links. We cannot view images on your computer. Please drag them from that folder into the body of a post to post them then reply.

@braydenkinkle7

As for the image that did make it are there any markings on it not visible in the image given?

I apologize these are the two photos that I was trying to post on the forum earlier. The white (what I believe are resistors) in the photo don’t have any markings on them. The only marking I could find was the R60A and R60B marking on the board itself. I identified the board to be from the model MUZ-A24NA outdoor air conditioning unit and found a pdf online which had some pcb schematics in it. Not sure if this will help with identification or is needed but this is where I found the pdf at. https://www.mitsubishitechinfo.ca/sites/default/files/SH_MU(Y)(Z)-(G)A09_24NA_OB451G\_(Parts).pdf

@braydenkinkle7

The link you gave seems to be broken.

One of the images you have shows the 1.1ΩG 2W
Which can be 1.1Ω 2% 2W if so we have an item that meets that.
696-PF2472-1R1F1-ND
PF2472-1R1F1 Riedon products by Bourns | Resistors | DigiKey

However if it is 1.1GΩ 2W the 2485-SM108031507FE-ND would be more similar.
SM108031507FE Ohmite | Resistors | DigiKey Marketplace

I’ve tried to attach the PDF through another link from the website. Would the white resistors be identifiable without any markings on them?

Not with the data I see so far.
The document you gave does not seem to have a bill of materials in it that would list items down to that level of component.