RF600526 - RFID tag range on non-metal surfaces

How is the range for part RF600526 on non-metal specified? It is not mentioned explicitly in the datasheet.


 

Image

MFR PART # RF600526
DIGIKEY PART # 1543-1002-ND
MANUFACTURER Avery Dennison RFID
DESCRIPTION RFID Tag Read/Write 128b (EPC) Memory 860MHz ~ 960MHz EPC, ISO 18000-6 Inlay
DATASHEET Click Here

 


The read distance is calculated in meters, by frequency on the two graphs at the bottom of page 2 of the datasheet.

It looks like the range is from .5 meters to a little over 4.6 meters


image
Avery Dennison RFID