Glass overcoat on chip and network resistors.
Unfortunately, these are not available anymore. What is important to know is that this is legacy technology that was improved upon by changing to the use of resins. This change helped the supplier lower costs on the series. The parts that originally used the glass overcoat were placed obsolete by the supplier and made unavailable. The link below will bring you to the PTN.
RHM-GLSRES-250118.pdf (2.1 MB)
To make this a little more clear, the overcoat is the highlighted portion of the resistor in the diagram below. There should not be any adverse reaction to using one of these resin parts in place of a legacy glass option.
These are the part numbers that were effected by the PTN:
It should be noted that even the parts that are considered alternatives by the supplier are currently listed as discontinued by DigiKey.
This link will show you what we have in stock
This link will show all numbers in the system.
ROHM SEMI CONDUCTORS | ROHM SUGGESTED ALTERNATIVE PART NUMBER |
---|---|
MCR01 MZS J | MCR01 MZP J |
MCR03 E6H J | MCR03 EZP J |
MCR03 EZH J | |
MCR03 QNH. J | |
MCR10 E6H J | MCR10 EZP J |
MCR10 EZH J | |
MCR10 EZH F | MCR10 EZP F |
MCR10 EZHD FX | |
MCR18 E6H J | MCR18 EZP J |
MCR18 EZH J | |
MCR18 FZH J | |
MCR18 EZH F | MCR18 EZP F |
MNR18 FZH F | |
MNR04 MOAB J | MNR04 M0AP J |
MNR14 E0AB J | MNR14 E0AP J |
MNR14 E6AB J |