After creating a very large circuit diagram in Scheme-It I have found myself going back to annotate and clean up some things. To do this I need to send things to the front and to the back in the arrangement queue found in the Object Properties tab of most entities. When working with a smaller circuit this isn’t a problem as I only need to click the Arrange:Front or Back buttons a small number of times. If I want to overlay something new underneath something I created at the beginning of my project with hundreds of entities, I have to click hundreds of times, or simply copy and paste (and rejoin) all of the connections I currently have in that region, to manually send it to the front of the arrangement queue. I know Microsoft Powerpoint has a feature similar to what I am suggesting, one button each for send forward and backward, and another two for send to the front and send to the back. These latter two would place whatever object/entity at the very beginning and ending of the drawing layers, respectively. This feature seems very easy to implement, and would offer a world of efficiency for the user.
Welcome to the Technical Forum. I am not able to find a solution to this one. This will go to the Scheme it team also. They will have to help.
First of all, thank you, Booleon, for using Scheme-it.
Thank you for your suggestion. We welcome all ideas for improvement so we will definitely take this suggestion under consideration.
Curtis Johnson