SCK 251R0 Thermistor Replacement Help

So, let me start off by saying that I’m a complete novice when it comes to thermistors, capacitors, ect. . My area of expertise is with building and repairing PCs and laptops, and being a competant solderer.

Anyways, my uncle whom works for an HVAC company brought me a Genteq 2.3 ECM CP04 motor with a shot thermistor. How hard could it be, I thought, figuring I would just type in the model number and viola!

How wrong I was.

Finding a replacement (I don’t care if its the same or different make, just that it works and works RIGHT) has been a nightmare. I’m not too savvy when it comes to ohms and voltages, so I could really use the help.

The matter is tracking down a suitable replacement, since I can handle the installation without issue.

Please look at part number 570-1041-ND as a possible replacement. The size is 22mm in stead of 25mm. The other values are the same.

Hi buddy, 25mm can be suitable for you and also easily accessable. So yea, you can give that a try.

Regards,
Smith