------Question for STEVAL-BFA001V2B Please Put your question below------
for product STEVAL-BFA001V2B Please let me know following;
1. Can I connect this sensor to my enclosure in 1/2" Npt and 3/4" Connection port? Anyone will be required at a time
2. is it explosion proof certified? As I need to supply this for Exd IIC T6 certified box
3. What is the dimension of this sensor
4. What accessories I need along with the sensor to get it’s realtime data continuously? Do we have to buy them separately? What are the rates for them? Can you give me a manual and step by step method to use it.
5. Can we get data wirelessly?
6. Do you also provide software along with the sensor to get logical graphs and monitor the data? If so any extra charge is there? Please provide more details on type of features and analysis we can do.
7. How much old data can be stored?
8. Any data security provision you have on your software?
9. Please provide contact details of your Ahmedabad, India office to personally visit and understand the product.
10. Do you have service support in Ahmedabad, India?
Hello boxsensetechnology and welcome to the DigiKey TechForum.
You can find extensive documentation regarding the product and software on the manufacturers page linked HERE.
Looking at the User Manual, it appears that the threading on this particular device is M12, you may be able to get an M12 to 1/2"NPT adapter and an M12 to 3/4" adapter, but it wouldn’t natively work with either of those threading.
I do not see that it has any certification related to being explosion proof.
The dimensions listed on the datasheet are 50x9x9mm.
According to the user manual this comes with the following.
• One STEVAL-IDP005V2(1) sensor node reference design (10 x 50 mm).
• One adapter for ST-LINK programming and debugging tool - STEVAL-UKI001V2.
• STLINK-V3MINI debugger/programmer for STM32 and STDC14 flat cable.
• One 0.050” 10-pin flat cable.
• One 4-pole cable with M12 female connector.
• One 4-pole mount M12 connector plug, with male contacts.
You will want to review the documentation listed on the software tab to ensure if it will work for your application.
The firmware section of one of the 2566 User Manual does state that Data Logging is capable through mobile app, so should be able to be viewed wirelessly.
In regard to 9 and 10, we do not have a satellite support office and do not offer on-site support.