Hello,
I need to source a green LED as in the attached picture. Would someone please be able to help me identifying the package type? I can measure a 2V voltage drop when they’re lit and they’re green.
Thanks!
Hello Tony359,
It appears that it may be a 2-SMD, Gull Wing similar to L62605CT-ND.
We also have the 2V, 2.1V, and 2.2V options linked HERE with a similar package.
Thank you Nick, very much appreciated.
I had a look and I think the ones I need to install is a “reverse gull wing” type as in the picture. I cannot find much on the Digikey catalogue, have you got something available?
The lens size seems to be around 1.7mm, round.
Thanks again!

Thank you Ryan,
I think one of them is the one! Cheers!