This guide is still good but should be updated to use the projects new name.
It goes by mediamtx now. All instructions but two still work just by changing the name.
Additionally the section on creating the service contains an error. The first and last lines of the text block to be copied into the nano editor should not be included.
My personal recommendation is to change the ‘nano’ command in the previous instruction to ‘touch’ to create the file and then use the command in the next block in the terminal window. If this is considered too risky just remove the first and last lines of that text block.
Any plans to update this guide??? Been trying to make this work, and it seems that more than just the name has been changed.
I’m stuck here: “Edit the source within the paths section of the file, change “all:” to “cam:” and the source to rpiCamera.”
A lot has changed since I wrote that guide, so I am working on an updated guide that takes a different approach to provide the same result with easier setup and lower overhead so it works better on the Pi Zero boards. It should be live in the upcoming weeks.