Hello,
I am trying to repair the mainboard of a Clarion CMS5 marine radio. Specifically, the controller knob/dial component became very rusted and needs replacing. The component is marked “ddm 427” which seems to be a DDM 427 Encoder made by ddm hopt+schuler in Germany. I was able to source this exact component but it is either quite expensive or I have to purchase it overseas so I was wondering if someone could help me identify a suitable replacement that could be purchased easily from places like Mouser/DigiKey and also isn’t so expensive? I have never worked with components like this before so I am unfamiliar with them or how to identify a suitable compatible replacement.
I am attaching several photos of the component itself from many angles as well as a photo of the board to show where that component goes. If you need any additional information, I will be glad to provide that. Just let me know. Thank you so much!
Does this DigiKey part seem like it’s compatible?
PEC11R-4220F-S0024
Hi @bvilletechwizards
Could you count how many detents/clicks it makes in one full turn of the shaft? The 427 comes in 30, 16, and 15-click versions.
427 Series Datasheet:
8879742746654.pdf (1.7 MB)
Hi bvilletechwizards,
From the datasheet that @jon_11475 found, it would appear that your shaft height above the bushing is 16mm and the bushing is 7.3mm tall, for a combined height of 23.3mm above the main body of the encoder.
The PEC11R-4220F-S0024 you found isn’t far off. The body dimensions and the pin spacing look essentially identical. However, according to it’s datasheet, the total height of shaft and bushing is only 20mm, as indicated by the “20” in the part number.
We don’t know whether your encoder had detents or how many pulses it produced per revolution, but those don’t affect the actual function of the circuitry at all, just the user feel.
Assuming you need something at least as tall as your part, the following are probably better options, as they have 25mm total height above the main body of the encoder:
Thank you so much for the replies! I tried to see how many detents/pulses it has when rotating the knob, but I couldn’t feel any and that’s probably due to the heavy corrosion/rust this component has suffered. Thanks @David_1528 for that breakdown and component suggestion. I think I am going to go with your recommendation and order the 18ppr version and hopefully that will fix this. Thanks again!
Just wanted to come back with an update. I received the part recommended by @David_1528 yesterday. Everything fit beautifully, however, the part that sticks out where the controller knob pushes onto is quite a bit longer than the original (nearly double the length!) so it makes the controller knob stick out farther from the unit than the original one, but other than that, it was a perfect fit.
I was doing this repair for a customer of mine so I didn’t have a way to test it as this radio goes into a boat and has a proprietary connections to power it. Customer just called me to tell me that he installed it and tested it out and it works beautifully so that component was exactly what I needed to fix it for my customer.
I had zero prior experience with marine radios and their components, so this was new territory for me. Couldn’t have done it without the help I received here, so I just wanted to come back to update and say thank you. Thanks!