Let me see if i have got this correct.
Deciding on which IC to chose is based on the leakage current of the capacitor(s) this IC is in parallel with. So in a 3s2p we have 3 PAIRS of caps. That would be 0.75mA (leakage current of one cap mentioned in datasheet) x 2 = 1.5mA. Otherwise 1500uA because the IC datasheet references the reading in micro amps.
So in an application dealing with super-capacitors or energy storage devices we would need the MOSFET to have maximum resistance at lower voltage and start to conduct when the voltage reaches closer to 2.7v and hence conduct with least resistance when the voltage reaches 2.7v. In post#12 (if i have understood the table) the table says, the Vth for ALD810019 is 1.9v. This would mean that at 1.9v at the gate, the MOSFET would conduct (or begin conducting) 1uA and as this 1.9v (Vgs) starts to increase so does the Ids (current flowing from Drain to Source) there by maintaining a constant voltage across its parallel capacitor.
Now what does the resistors do here ? Dissipate the extra current as heat ? if yes then they would be in placed in parallel with drain and source of the conducting drain and source ?
Sorry about the long write-up, just making sure i understand the working of the IC before i go ahead with implementation.