Switchcraft slide switch come with screws?!

Switchcraft slide switch come with screws?

Screws would not be included.

Can i get the screws at Digikey?

Certainly. Our screws can be found here.

Which ones exactly do I need for the following, specific slide switch: 46313LDRX

I bought a bag of them from you all an 20 screws are not included. I have zero clue which screw from your link, I need to now buy!

Your switch hole diameter is 0.140inch.

The closest standard screw thread diameter is #6-32 but the length of screw needed depends upon the panel thickness you’re installing in the switch in.

What is the thickness of the material?

1/5th inches in thickness.

Below Head Height of 0.375 (3/8ths) inch

9904 Keystone Electronics | Hardware, Fasteners, Accessories | DigiKey

Here is a nut in case you need them:

4701 Keystone Electronics | Hardware, Fasteners, Accessories | DigiKey

I apologize. I got out the digital caliper and it measure 2.7mm in thickness to what the other, comparative slide switches are going through….

The suggested screw would work, it would just be 0.1inch (2.54mm) longer than you require.