Understanding Optocoupler Biasing for Stable Isolated SMPS Feedback

Introduction

In switch-mode power supply (SMPS) designs, optocouplers are critical components for enabling safe and reliable signal transmission across galvanic isolation boundaries. To work well, they need to be correctly connected and used in the feedback loop. If not set up properly, they can lead to instability, poor transient response, and degraded regulation.
This article explains how to correctly bias optocouplers—covering LED current, current transfer ratio (CTR), and phototransistor setup—to keep your power supply accurate, stable, and reliable.

What is an Optocoupler?

An optocoupler is an electronic component that basically acts as an interface between two separate circuits with different voltage levels while providing electrical isolation (Galvanic isolation) between them.
It is used to protect low voltage circuits from high voltage circuits by preventing hazardous current flow and eliminating unwanted noise.

Optocouplers, Optoisolators | Electronic Components Distributor DigiKey
image

Role of optocouplers in isolated feedback loops

In isolated switch-mode power supply (SMPS) architectures, feedback from the output (secondary) side to the input (primary) side must be transmitted without compromising electrical isolation. This can be achieved by using an optocoupler paired with a precision shunt regulator such as LT1431.
This shunt regulator monitors the SMPS output voltage through a resistor divider and adjusts the current flowing through the optocoupler’s LED to correct any deviation from the desired voltage setpoint.
The LED in the optocoupler emits light in proportion to the forward current (IF). This light is detected by a phototransistor on the primary side, which adjusts the control signal - typically at the PWM controller’s compensation pin (COMP). This modulation influences the duty cycle of the switching controller, forming a closed-loop feedback system that helps maintain stable output voltage under varying load and input conditions.

The performance of this feedback loop depends heavily on the optocoupler’s biasing and the design of the compensation network.
Poor biasing can lead to nonlinearity, saturation, or slow response, while an improperly tuned compensation network may cause instability or oscillation.

Optocoupler Biasing

Biasing of an optocoupler means setting the correct operating conditions specifically, the forward current through the LED, the collector-emitter voltage and current of the phototransistor so that the optocoupler operates in its linear region.
This is especially important in feedback systems, where the optocoupler needs to accurately transfer analog signals across an isolation barrier.

In an isolated SMPS (Switched-Mode Power Supply), the optocoupler acts as a bridge between the secondary-side voltage sensing and the primary-side PWM controller. If it’s not correctly biased, the feedback signal can become distorted, leading to poor voltage regulation or even instability.

Figure 1 shows the internal structure of the optocoupler and how it’s connected externally when used as a feedback element in an SMPS.

1. LED Side: Driving the Light (Input Stage)

In an SMPS with isolated feedback, the LED side of the optocoupler is typically driven by a shunt regulator (such as the LT1431), which adjust the LED’s forward current based on the output voltage.

Why Forward Current Matters?

The forward current through the LED determines the intensity of light it emits, which in turn controls how much the phototransistor conducts on the primary side.
The LED operates in the forward-biased region, and its light output increases with higher IF, for most designs, a forward current between 1 mA and 10 mA is recommended:

  • Too low (e.g., <1 mA): Insufficient optical power, leading to weak phototransistor activation and poor feedback regulation.
  • Too high (e.g., >10 mA): Can cause thermal stress, reduce lifetime, and degrade optical efficiency.

In practical designs, the LED current is set by a resistor (R2) at the LED anode, and this current dynamically adjusts as the shunt regulator adjusts its cathode current in response to output voltage changes.

Design Tip:

In high performance or fast transient SMPS designs, maintaining a stable and well-controlled IF is essential to ensure accurate, low noise, and thermally reliable operation of the optocoupler feedback path.
Designers must also consider the LED’s forward voltage drop when calculating headroom, especially on low-voltage rails.

Example: EL3H7(B)(TA)-VG (OPTOISO 3.75KV 1CH TRANS 4-SSOP)
This graph shows the design recommendation to operate the LED within a safe and linear range (typically 1–10 mA) to ensure stable and predictable feedback.

2. Understanding Current Transfer Ratio (CTR)

The current transfer ratio (CTR) is another parameter in optocoupler selection. It is defined as the ratio of the phototransistor output current to the LED input current, typically expressed as a percentage.

CTR (%) = (Phototransistor Output Current / LED Input Current) × 100

A CTR of 100% means 1 mA of LED current yields 1 mA of collector current at the phototransistor.

Why CTR Is Not a Constant

CTR varies with:

  • Temperature: Often decreases at high temperatures
  • LED current: Nonlinear at low currents
  • Aging: Light output degrades over time
  • Device variation: Some parts have wide CTR ranges (e.g., 50–600%)
    For example, the PC817D optocoupler offers CTR ranging from 50% to 600%, depending on the specific part number and operating conditions

Key Considerations when Selecting CTR

Designers must account for the minimum guaranteed CTR to ensure the feedback loop remains functional even under worst-case conditions.

  • If the CTR drops too low - due to temperature drift, aging, or manufacturing variation - the phototransistor may not provide enough current to drive the PWM controller’s compensation pin (COMP), leading to poor voltage regulation or even instability. For example, CTR typically decreases as temperature increases, which can reduce loop gain and cause sluggish response or loss of control at high temperatures. Similarly, long-term operation at high LED currents can degrade the LED’s efficiency, reducing light output and weakening the feedback signal.
  • Another critical factor is linearity. The optocoupler must operate in its linear region to ensure predictable feedback behavior. If the LED current causes the phototransistor to enter a nonlinear region—where small changes in input result in disproportionate changes in output—the feedback signal becomes distorted. This complicates compensation design and can lead to unstable or inaccurate voltage regulation.

By carefully considering these factors, designers can ensure that the optocoupler-based feedback loop remains robust, accurate, and stable throughout the product’s operating life and environmental conditions. For feedback applications, a tighter CTR tolerance (for example, 100% to 200%) is preferred to maintain consistent loop gain and predictable behavior.

Example Device EL3H7(B)(TA)-VG (OPTOISO 3.75KV 1CH TRANS 4-SSOP)
This graph shows how temperature drift affects CTR - CTR varies with forward current - lower IF values show sharper CTR drop with temperature, while higher IF values offer more stable CTR but still peak and decline.

3. Phototransistor Side: Receiving the Signal (Output Stage)

The phototransistor serves as the key element that converts the optical signal from the internal LED into an electrical output.
It is commonly configured in a common-emitter arrangement, the phototransistor has its emitter grounded and its collector connected to a pull-up resistor (R1), which defines the output voltage swing.

Collector Current Controls the COMP Pin

When the LED inside the optocoupler is forward-biased, it emits infrared light that hits the base region of the phototransistor, causing it to conduct. The resulting collector current (IC) is proportional to both the LED’s forward current and the optocoupler’s Current Transfer Ratio (CTR).

As the LED illumination increases, the phototransistor conducts more, causing its collector voltage to drop. This produces a low-level output signal, which is critical in isolated feedback systems like SMPS. In such systems, the phototransistor’s collector is often connected to the COMP pin or feedback input of the PWM controller. The voltage at this node directly affects the controller’s duty cycle, helping regulate the output voltage or current.

Pull-Up Resistor Effects

The pull-up resistor on the collector not only sets the high level output voltage when the transistor is off but also impacts the dynamic response of the feedback loop.

  • A lower resistance value can improve response time but may reduce voltage swing.
  • While a higher value increases swing but can slow down transitions.

Additionally, the phototransistor’s switching speed, saturation characteristics, and leakage current in the off state are important design considerations, especially in high frequency or precision applications.

Conclusion

Optocouplers may look a simple electronics device, just a light source and a transistor — but in SMPS feedback loops, they play a critical role. If the signal they pass across the isolation barrier is weak or delayed, the whole control system can become unstable.
Proper optocoupler biasing ensures accurate feedback in SMPS. The LED must operate within its ideal current range, and the phototransistor must reliably drive the PWM controller. Choosing a device with tight CTR tolerance and accounting for temperature and aging effects helps maintain stable regulation. Following datasheet guidelines and testing across conditions ensures long-term performance.
Optocoupler biasing is not just a matter of turning on a light. It’s about tuning a critical analog link in a high-speed control system. Mastering this ensures your SMPS design is not only functional but also reliable and efficient.

Coming Up

In the next article, we’ll explore compensation network design in isolated SMPS loops. You’ll learn how to:

  • Select and design Type II or Type III compensation
  • Set crossover frequency and phase margin
  • Account for optocoupler bandwidth and nonlinearities
Applicable Part Numbers
DigiKey Part Number Manufacturer Part Number
LT1431CS8#TRPBFTR-ND,LT1431CS8#TRPBFCT-ND,LT1431CS8#TRPBFDKR-ND LT1431CS8#TRPBF
LT1431IS8#TRPBFTR-ND,LT1431IS8#TRPBFCT-ND,LT1431IS8#TRPBFDKR-ND LT1431IS8#TRPBF
LT1431MPS8#PBF-ND LT1431MPS8#PBF
505-LT1431IZ#PBF-ND LT1431IZ#PBF
LT1431CS8#PBF-ND LT1431CS8#PBF
LT1431IS8#PBF-ND LT1431IS8#PBF
LT1431CZ#PBF-ND LT1431CZ#PBF
LT1431CN8#PBF-ND LT1431CN8#PBF
LT1431IN8#PBF-ND LT1431IN8#PBF
2156-LT1431IN8#PBF-ND LT1431IN8#PBF
LT1431IZ#TRPBF-ND LT1431IZ#TRPBF
505-LT1431MPS8#TRPBFTR-ND LT1431MPS8#TRPBF
LT1431CN8-ND LT1431CN8
LT1431CS8-ND LT1431CS8
LT1431CS8TR-ND LT1431CS8#TR
LT1431IN8-ND LT1431IN8
LT1431IS8-ND LT1431IS8
LT1431CZ#AMMO-ND LT1431CZ#AMMO
LT1431IZ#TR-ND LT1431IZ#TR
LT1431CZ#TR-ND LT1431CZ#TR
LT1431IS8#TR-ND LT1431IS8#TR
LT1431CZ#TRPBF-ND LT1431CZ#TRPBF
LT1431MJ8-ND LT1431MJ8
160-1367-5-ND LTV-817S
160-1361-5-ND LTV-816S
160-1893-2-ND,160-1893-1-ND,160-1893-6-ND LTV-817S-TA1
1080-1197-2-ND,1080-1197-1-ND,1080-1197-6-ND EL3H7(B)(TA)-VG
160-1337-2-ND,160-1337-1-ND,160-1337-6-ND LTV-356T
160-1339-2-ND,160-1339-1-ND,160-1339-6-ND LTV-357T
160-1911-2-ND,160-1911-1-ND,160-1911-6-ND 4N35S-TA1
160-1892-2-ND,160-1892-1-ND,160-1892-6-ND LTV-816S-TA1
VO618A-3X017TTR-ND,VO618A-3X017TCT-ND,VO618A-3X017TDKR-ND VO618A-3X017T
160-LTV-817S-TA1-ATR-ND,160-LTV-817S-TA1-ACT-ND,160-LTV-817S-TA1-ADKR-ND LTV-817S-TA1-A
1080-1198-2-ND,1080-1198-1-ND,1080-1198-6-ND EL3H7(TA)-VG
58-ISP281DTR-ND,58-ISP281DCT-ND,58-ISP281DDKR-ND ISP281D
751-1267-5-ND CNY17-3
1080-1537-2-ND,1080-1537-1-ND,1080-1537-6-ND EL3H7(C)(TA)-VG
160-1335-2-ND,160-1335-1-ND,160-1335-6-ND LTV-355T
160-LTV-356T-BTR-ND,160-LTV-356T-BCT-ND,160-LTV-356T-BDKR-ND LTV-356T-B
TLP291(GB-TPSETR-ND,TLP291(GB-TPSECT-ND,TLP291(GB-TPSEDKR-ND TLP291(GB-TP,SE
160-2040-2-ND,160-2040-1-ND,160-2040-6-ND LTV-827S-TA1
TLP291(GBSE-ND TLP291(GB,SE
TLP185(GB-TPLSETR-ND,TLP185(GB-TPLSECT-ND,TLP185(GB-TPLSEDKR-ND TLP185(GB-TPL,SE
TLP291(BLL-TPSETR-ND,TLP291(BLL-TPSECT-ND,TLP291(BLL-TPSEDKR-ND TLP291(BLL-TP,SE
TLP291(GR-TPSETR-ND,TLP291(GR-TPSECT-ND,TLP291(GR-TPSEDKR-ND TLP291(GR-TP,SE
TLP291(BL-TPSETR-ND,TLP291(BL-TPSECT-ND,TLP291(BL-TPSEDKR-ND TLP291(BL-TP,SE
FOD817A3SDTR-ND,FOD817A3SDCT-ND,FOD817A3SDDKR-ND FOD817A3SD
FOD817D3SDTR-ND,FOD817D3SDCT-ND,FOD817D3SDDKR-ND FOD817D3SD
FOD817DSDTR-ND,FOD817DSDCT-ND,FOD817DSDDKR-ND FOD817DSD
160-1333-2-ND,160-1333-1-ND,160-1333-6-ND LTV-354T
TLP183(BL-TPLETR-ND,TLP183(BL-TPLECT-ND,TLP183(BL-TPLEDKR-ND TLP183(BL-TPL,E
TLP293(GB-TPLETR-ND,TLP293(GB-TPLECT-ND,TLP293(GB-TPLEDKR-ND TLP293(GB-TPL,E
TLP293(GR-TPLETR-ND,TLP293(GR-TPLECT-ND,TLP293(GR-TPLEDKR-ND TLP293(GR-TPL,E
160-1891-2-ND,160-1891-1-ND,160-1891-6-ND LTV-814S-TA1
160-2256-2-ND,160-2256-1-ND,160-2256-6-ND LTV-814S-TA
TLP183(TPLETR-ND,TLP183(TPLECT-ND,TLP183(TPLEDKR-ND TLP183(TPL,E
TLP183(GB-TPLETR-ND,TLP183(GB-TPLECT-ND,TLP183(GB-TPLEDKR-ND TLP183(GB-TPL,E
TLP293(GRL-TPLETR-ND,TLP293(GRL-TPLECT-ND,TLP293(GRL-TPLEDKR-ND TLP293(GRL-TPL,E
TLP293(BL-TPLETR-ND,TLP293(BL-TPLECT-ND,TLP293(BL-TPLEDKR-ND TLP293(BL-TPL,E
FOD817B3SDTR-ND,FOD817B3SDCT-ND,FOD817B3SDDKR-ND FOD817B3SD
VOS617A-3TTR-ND,VOS617A-3TCT-ND,VOS617A-3TDKR-ND VOS617A-3T
VOS618A-3TTR-ND,VOS618A-3TCT-ND,VOS618A-3TDKR-ND VOS618A-3T
VOS617A-4TTR-ND,VOS617A-4TCT-ND,VOS617A-4TDKR-ND VOS617A-4T
516-2722-2-ND,516-2722-1-ND,516-2722-6-ND HCPL-817-500E
VOS618A-3X001TTR-ND,VOS618A-3X001TCT-ND,VOS618A-3X001TDKR-ND VOS618A-3X001T
516-2580-2-ND,516-2580-1-ND,516-2580-6-ND HCPL-817-50DE
751-1346-2-ND,751-1346-1-ND,751-1346-6-ND SFH6156-2T
VOS617A-3X001TTR-ND,VOS617A-3X001TCT-ND,VOS617A-3X001TDKR-ND VOS617A-3X001T
751-1348-2-ND,751-1348-1-ND,751-1348-6-ND SFH6156-4T
VOS617A-7X001TTR-ND,VOS617A-7X001TCT-ND,VOS617A-7X001TDKR-ND VOS617A-7X001T
VOS617A-7TTR-ND,VOS617A-7TCT-ND,VOS617A-7TDKR-ND VOS617A-7T
TLP292(GB-TPLETR-ND,TLP292(GB-TPLECT-ND,TLP292(GB-TPLEDKR-ND TLP292(GB-TPL,E
TLP182(BL-TPLETR-ND,TLP182(BL-TPLECT-ND,TLP182(BL-TPLEDKR-ND TLP182(BL-TPL,E
160-2036-2-ND,160-2036-1-ND,160-2036-6-ND LTV-814HS-TA1
MOCD207M-ND MOCD207M
FOD814ASDTR-ND,FOD814ASDCT-ND,FOD814ASDDKR-ND FOD814ASD
VOL618A-3TTR-ND,VOL618A-3TCT-ND,VOL618A-3TDKR-ND VOL618A-3T
FODM121R2TR-ND,FODM121R2CT-ND,FODM121R2DKR-ND FODM121R2
751-TCMT1109TR-ND,751-TCMT1109CT-ND,751-TCMT1109DKR-ND TCMT1109
FODM217AR2OSTR-ND,FODM217AR2OSCT-ND,FODM217AR2OSDKR-ND FODM217AR2
TCMT1106TR-ND,TCMT1106CT-ND,TCMT1106DKR-ND TCMT1106
TCMT1100TR-ND,TCMT1100CT-ND,TCMT1100DKR-ND TCMT1100
FODM124R2TR-ND,FODM124R2CT-ND,FODM124R2DKR-ND FODM124R2
751-TCMT1103TR-ND,751-TCMT1103CT-ND,751-TCMT1103DKR-ND TCMT1103
TCMT1107TR-ND,TCMT1107CT-ND,TCMT1107DKR-ND TCMT1107
488-FODM217BR2TR-ND,488-FODM217BR2CT-ND,488-FODM217BR2DKR-ND FODM217BR2
516-1787-2-ND,516-1787-1-ND,516-1787-6-ND HCPL-181-00BE
516-1646-2-ND,516-1646-1-ND,516-1646-6-ND HCPL-181-000E
516-1788-2-ND,516-1788-1-ND,516-1788-6-ND HCPL-181-00CE
FOD814SDTR-ND,FOD814SDCT-ND,FOD814SDDKR-ND FOD814SD
160-2035-2-ND,160-2035-1-ND,160-2035-6-ND LTV-8141S-TA1
160-1331-2-ND,160-1331-1-ND,160-1331-6-ND LTV-352T
516-2893-2-ND,516-2893-1-ND,516-2893-6-ND ACPL-217-50BE
516-1978-2-ND,516-1978-1-ND,516-1978-6-ND ACPL-217-500E
516-2894-2-ND,516-2894-1-ND,516-2894-6-ND ACPL-217-50DE
HMHA2801R2TR-ND,HMHA2801R2CT-ND,HMHA2801R2DKR-ND HMHA2801R2
FODM2705R2TR-ND,FODM2705R2CT-ND,FODM2705R2DKR-ND FODM2705R2
160-1790-2-ND,160-1790-1-ND,160-1790-6-ND 6N136S-TA1
516-2896-2-ND,516-2896-1-ND,516-2896-6-ND ACPL-217-56BE
TCLT1003TR-ND,TCLT1003CT-ND,TCLT1003DKR-ND TCLT1003
TCLT1009TR-ND,TCLT1009CT-ND,TCLT1009DKR-ND TCLT1009
VOS627A-X001TTR-ND,VOS627A-X001TCT-ND,VOS627A-X001TDKR-ND VOS627A-X001T
HMHA281R2TR-ND,HMHA281R2CT-ND,HMHA281R2DKR-ND HMHA281R2
TCLT1600TR-ND,TCLT1600CT-ND,TCLT1600DKR-ND TCLT1600
TCMD1000TR-ND,TCMD1000CT-ND,TCMD1000DKR-ND TCMD1000
751-1374-2-ND,751-1374-1-ND,751-1374-6-ND TCMT1600
516-2988-2-ND,516-2988-1-ND,516-2988-6-ND HCPL-354-06AE
559-1127-ND PS2501L-1-L-A
1855-1004-2-ND,1855-1004-1-ND,1855-1004-6-ND PC357N1J000F
MOC207R2MTR-ND,MOC207R2MCT-ND,MOC207R2MDKR-ND MOC207R2M
516-2218-2-ND,516-2218-1-ND,516-2218-6-ND ACPL-214-500E
1855-1023-2-ND,1855-1023-1-ND,1855-1023-6-ND PC357NJ0000F
1855-1005-2-ND,1855-1005-1-ND,1855-1005-6-ND PC357N2J000F
1855-1022-2-ND,1855-1022-1-ND,1855-1022-6-ND PC357N4J000F
1855-1006-2-ND,1855-1006-1-ND,1855-1006-6-ND PC357N3J000F
TLP188(TPLETR-ND,TLP188(TPLECT-ND,TLP188(TPLEDKR-ND TLP188(TPL,E
559-1038-2-ND,559-1038-1-ND,559-1038-6-ND PS2801C-1-F3-A
IS127TR-ND,IS127CT-ND,IS127DKR-ND IS127
MCT62-ND MCT62
160-1365-5-ND LTV-846S
MCT6-ND MCT6
1855-1034-2-ND,1855-1034-1-ND,1855-1034-6-ND PC354NJ0000F
MOCD213M-ND MOCD213M
MOCD217M-ND MOCD217M
MOCD213R2MTR-ND,MOCD213R2MCT-ND,MOCD213R2MDKR-ND MOCD213R2M
559-1027-2-ND,559-1027-1-ND,559-1027-6-ND PS2702-1-F3-A
FOD8523SDTR-ND,FOD8523SDCT-ND,FOD8523SDDKR-ND FOD8523SD
MCT9001SDTR-ND,MCT9001SDCT-ND,MCT9001SDDKR-ND MCT9001SD
559-1154-2-ND,559-1154-1-ND,559-1154-6-ND PS2701A-1-F3-A
559-1155-2-ND,559-1155-1-ND,559-1155-6-ND PS2703-1-F3-A
MCT62SDTR-ND,MCT62SDCT-ND,MCT62SDDKR-ND MCT62SD
FOD852SDTR-ND,FOD852SDCT-ND,FOD852SDDKR-ND FOD852SD
1855-1007-2-ND,1855-1007-1-ND,1855-1007-6-ND PC3H710NIP1H
160-1371-5-ND LTV-847S
559-1050-2-ND,559-1050-1-ND,559-1050-6-ND PS2811-1-F3-A
TLP187(TPLETR-ND,TLP187(TPLECT-ND,TLP187(TPLEDKR-ND TLP187(TPL,E
160-1370-5-ND LTV-847
MOCD207R2MTR-ND,MOCD207R2MCT-ND,MOCD207R2MDKR-ND MOCD207R2M
751-1288-2-ND,751-1288-1-ND,751-1288-6-ND IL217AT
160-2255-2-ND,160-2255-1-ND,160-2255-6-ND LTV-247
MOCD223M-ND MOCD223M
1855-1024-2-ND,1855-1024-1-ND,1855-1024-6-ND PC364NJ0000F
1080-1200-2-ND,1080-1200-1-ND,1080-1200-6-ND ELD207(TA)-V
MOCD223R2MTR-ND,MOCD223R2MCT-ND,MOCD223R2MDKR-ND MOCD223R2M
1855-1025-2-ND,1855-1025-1-ND,1855-1025-6-ND PC365NJ0000F
559-1031-2-ND,559-1031-1-ND,559-1031-6-ND PS2705A-1-F3-A
516-2616-2-ND,516-2616-1-ND,516-2616-6-ND ACPL-227-500E
160-2041-5-ND LTV-845
516-ACPL-227-50CETR-ND,516-ACPL-227-50CECT-ND,516-ACPL-227-50CEDKR-ND ACPL-227-50CE
TLP109(TPLETR-ND,TLP109(TPLECT-ND,TLP109(TPLEDKR-ND TLP109(TPL,E
160-2042-5-ND LTV-845S
751-1312-2-ND,751-1312-1-ND,751-1312-6-ND ILD213T
559-1032-2-ND,559-1032-1-ND,559-1032-6-ND PS2706-1-F3-A
SFH619A-X007TTR-ND,SFH619A-X007TCT-ND,SFH619A-X007TDKR-ND SFH619A-X007T
160-1349-5-ND LTV-844S
751-1313-2-ND,751-1313-1-ND,751-1313-6-ND ILD217T
ILD1207TTR-ND,ILD1207TCT-ND,ILD1207TDKR-ND ILD1207T
TLP291-4(TPE)TR-ND,TLP291-4(TPE)CT-ND,TLP291-4(TPE)DKR-ND TLP291-4(TP,E)
TLP291-4(GB-TPE)TR-ND,TLP291-4(GB-TPE)CT-ND,TLP291-4(GB-TPE)DKR-ND TLP291-4(GB-TP,E)
559-1041-2-ND,559-1041-1-ND,559-1041-6-ND PS2802-1-F3-A
559-1018-ND PS2506-1-A
IS281-4TR-ND,IS281-4CT-ND,IS281-4DKR-ND IS281-4
516-3753-2-ND,516-3753-1-ND,516-3753-6-ND ACPL-224-500E
751-1261-5-ND 6N136
H11F1M-ND H11F1M
H11F1SM-ND H11F1SM
212-CPC1001NTR-ND,212-CPC1001NTRCT-ND,212-CPC1001NTRDKR-ND CPC1001NTR
IS2801-4TR-ND,IS2801-4CT-ND,IS2801-4DKR-ND IS2801-4
TLP290-4(GB-TPE)TR-ND,TLP290-4(GB-TPE)CT-ND,TLP290-4(GB-TPE)DKR-ND TLP290-4(GB-TP,E)
IS281-4GBTR-ND,IS281-4GBCT-ND,IS281-4GBDKR-ND IS281-4GB
TLP290-4(TPETR-ND,TLP290-4(TPECT-ND,TLP290-4(TPEDKR-ND TLP290-4(TP,E
TLP293-4(V4GBTPETR-ND,TLP293-4(V4GBTPECT-ND,TLP293-4(V4GBTPEDKR-ND TLP293-4(V4GBTPE
TLP293-4(LGBTPETR-ND,TLP293-4(LGBTPECT-ND,TLP293-4(LGBTPEDKR-ND TLP293-4(LGBTP,E
TLP293-4(GB-TPETR-ND,TLP293-4(GB-TPECT-ND,TLP293-4(GB-TPEDKR-ND TLP293-4(GB-TP,E
TLP293-4(TPETR-ND,TLP293-4(TPECT-ND,TLP293-4(TPEDKR-ND TLP293-4(TP,E
TLP293-4(LGBTRETR-ND,TLP293-4(LGBTRECT-ND,TLP293-4(LGBTREDKR-ND TLP293-4(LGBTR,E
TLP293-4(GBE-ND TLP293-4(GB,E
255-3874-2-ND,255-3874-1-ND,255-3874-6-ND APV2111VY
516-1601-5-ND 6N139-000E
H11F1SR2MTR-ND,H11F1SR2MCT-ND,H11F1SR2MDKR-ND H11F1SR2M
FODM8801CR2TR-ND,FODM8801CR2CT-ND,FODM8801CR2DKR-ND FODM8801CR2
516-6N139-500ETR-ND,516-6N139-500ECT-ND,516-6N139-500EDKR-ND 6N139-500E
TLP292-4(GB-TPETR-ND,TLP292-4(GB-TPECT-ND,TLP292-4(GB-TPEDKR-ND TLP292-4(GB-TP,E
TLP292-4(LGBTPETR-ND,TLP292-4(LGBTPECT-ND,TLP292-4(LGBTPEDKR-ND TLP292-4(LGBTP,E
PS2501-4XSM-ND PS2501-4XSM
264-TLP3905(TPL,ETR-ND,264-TLP3905(TPL,ECT-ND,264-TLP3905(TPL,EDKR-ND TLP3905(TPL,E
TLP3906(TPLETR-ND,TLP3906(TPLECT-ND,TLP3906(TPLEDKR-ND TLP3906(TPL,E
FODM8801CFS-ND FODM8801C
VOM1271TTR-ND,VOM1271TCT-ND,VOM1271TDKR-ND VOM1271T
TCMT4100T0TR-ND,TCMT4100T0CT-ND,TCMT4100T0DKR-ND TCMT4100T0
VOMA617A-3X001TTR-ND,VOMA617A-3X001TCT-ND,VOMA617A-3X001TDKR-ND VOMA617A-3X001T
751-1375-2-ND,751-1375-1-ND,751-1375-6-ND TCMT4100
516-2176-5-ND ACPL-847-300E
1855-1035-2-ND,1855-1035-1-ND,1855-1035-6-ND PC452J00000F
255-3339-2-ND,255-3339-1-ND,255-3339-6-ND APV1121SX
559-1022-2-ND,559-1022-1-ND,559-1022-6-ND PS2533L-1-F3-A
IS2805-4TR-ND,IS2805-4CT-ND,IS2805-4DKR-ND IS2805-4
FODM8801CR2VTR-ND,FODM8801CR2VCT-ND,FODM8801CR2VDKR-ND FODM8801CR2V
160-1914-2-ND,160-1914-1-ND,160-1914-6-ND CNY17-4S-TA1
516-2466-2-ND,516-2466-1-ND,516-2466-6-ND ACPL-247-500E
255-5976-2-ND,255-5976-1-ND,255-5976-6-ND APV2111VW
559-1061-2-ND,559-1061-1-ND,559-1061-6-ND PS2913-1-F3-AX
559-1056-2-ND,559-1056-1-ND,559-1056-6-ND PS2833-1-F3-A
516-2219-2-ND,516-2219-1-ND,516-2219-6-ND ACPL-247-560E
5656-CPC1301GRTR-ND,5656-CPC1301GRTRCT-ND,5656-CPC1301GRTRDKR-ND CPC1301GRTR
751-1376-2-ND,751-1376-1-ND,751-1376-6-ND TCMT4600
751-TCMD4000TR-ND,751-TCMD4000CT-ND,751-TCMD4000DKR-ND TCMD4000
VOMA617A-X001TTR-ND,VOMA617A-X001TCT-ND,VOMA617A-X001TDKR-ND VOMA617A-X001T
TCMT4600T0TR-ND,TCMT4600T0CT-ND,TCMT4600T0DKR-ND TCMT4600T0
516-1612-5-ND HCNW139-000E
559-1062-2-ND,559-1062-1-ND,559-1062-6-ND PS2915-1-F3-AX
516-4191-2-ND,516-4191-1-ND,516-4191-6-ND HCNW139-500E
1855-1036-2-ND,1855-1036-1-ND,1855-1036-6-ND PC457L0NIP0F
516-1529-2-ND,516-1529-1-ND,516-1529-6-ND HCPL-0501-500E
516-2971-2-ND,516-2971-1-ND,516-2971-6-ND HCPL-0453-500E
FODM452R2TR-ND,FODM452R2CT-ND,FODM452R2DKR-ND FODM452R2
516-2696-2-ND,516-2696-1-ND,516-2696-6-ND HCNW136-500E
HCPL2731SDMTR-ND,HCPL2731SDMCT-ND,HCPL2731SDMDKR-ND HCPL2731SDM
516-2898-2-ND,516-2898-1-ND,516-2898-6-ND ACPL-244-500E
559-1040-2-ND,559-1040-1-ND,559-1040-6-ND PS2801C-4-F3-A
255-2656-ND APV1121S
516-2515-2-ND,516-2515-1-ND,516-2515-6-ND HCPL-4503-500E
516-1637-5-ND HCPL-0701-000E
516-1488-2-ND,516-1488-1-ND,516-1488-6-ND HCPL-0701-500E
516-3754-2-ND,516-3754-1-ND,516-3754-6-ND ACPL-244-560E
HCPL0701R2TR-ND,HCPL0701R2CT-ND,HCPL0701R2DKR-ND HCPL0701R2
CNY65STTR-ND,CNY65STCT-ND,CNY65STDKR-ND CNY65ST
516-4227-2-ND,516-4227-1-ND,516-4227-6-ND HCPL-M452-500E
559-1063-2-ND,559-1063-1-ND,559-1063-6-ND PS8101-F3-AX
751-1370-5-ND SFH6916
365-1032-ND OPI1264B
365-1033-ND OPI1264C
516-2727-2-ND,516-2727-1-ND,516-2727-6-ND HCPL-M453-500E
5656-LOC110STR-ND,5656-LOC110STRCT-ND,5656-LOC110STRDKR-ND LOC110STR
CNY65AGRSTTR-ND,CNY65AGRSTCT-ND,CNY65AGRSTDKR-ND CNY65AGRST
CNY65AYSTTR-ND,CNY65AYSTCT-ND,CNY65AYSTDKR-ND CNY65AYST
516-2908-2-ND,516-2908-1-ND,516-2908-6-ND ACPL-M49T-500E
212-LOC110-ND LOC110
HCPL0731-ND HCPL0731
HCPL0731R2TR-ND,HCPL0731R2CT-ND,HCPL0731R2DKR-ND HCPL0731R2
516-1474-5-ND HCPL-2531-000E
IL300-DEFG-X007-ND IL300-DEFG-X007
IL300-DEFG-X007TTR-ND,IL300-DEFG-X007TCT-ND,IL300-DEFG-X007TDKR-ND IL300-DEFG-X007T
264-TLX9000(TPLFTR-ND,264-TLX9000(TPLFCT-ND,264-TLX9000(TPLFDKR-ND TLX9000(TPL,F
264-TLX9291A(GBTPLFTR-ND,264-TLX9291A(GBTPLFCT-ND,264-TLX9291A(GBTPLFDKR-ND TLX9291A(GBTPL,F
264-TLX9300(TPLFTR-ND,264-TLX9300(TPLFCT-ND,264-TLX9300(TPLFDKR-ND TLX9300(TPL,F
264-TLX9185A(GBTPLFTR-ND,264-TLX9185A(GBTPLFCT-ND,264-TLX9185A(GBTPLFDKR-ND TLX9185A(GBTPL,F
516-2707-2-ND,516-2707-1-ND,516-2707-6-ND HCPL-2531-500E
5656-LOC111PTR-ND,5656-LOC111PTRCT-ND,5656-LOC111PTRDKR-ND LOC111PTR
516-2969-2-ND,516-2969-1-ND,516-2969-6-ND HCNW4503-500E
516-1621-5-ND HCNW4503-300E
559-1103-2-ND,559-1103-1-ND,559-1103-6-ND PS2802-4-F3-A
5656-LOC111-ND LOC111
LH1262CACTRTR-ND,LH1262CACTRCT-ND,LH1262CACTRDKR-ND LH1262CACTR
516-ACPL-K70A-500ETR-ND,516-ACPL-K70A-500ECT-ND,516-ACPL-K70A-500EDKR-ND ACPL-K70A-500E
751-1293-5-ND IL300-DEFG
516-ACPL-K70A-560ETR-ND,516-ACPL-K70A-560ECT-ND,516-ACPL-K70A-560EDKR-ND ACPL-K70A-560E
559-1053-2-ND,559-1053-1-ND,559-1053-6-ND PS2811-4-F3-A
516-2237-2-ND,516-2237-1-ND,516-2237-6-ND ACPL-M43T-500E
516-1543-5-ND HCPL-2731-000E
516-2698-2-ND,516-2698-1-ND,516-2698-6-ND HCPL-0530-500E
559-PS2815-4-F3-ATR-ND,559-PS2815-4-F3-ACT-ND,559-PS2815-4-F3-ADKR-ND PS2815-4-F3-A
264-TLX9906(TPLFTR-ND,264-TLX9906(TPLFCT-ND,264-TLX9906(TPLFDKR-ND TLX9906(TPL,F
516-1530-5-ND HCPL-0531-000E
516-1484-2-ND,516-1484-1-ND,516-1484-6-ND HCPL-0531-500E
516-3223-2-ND,516-3223-1-ND,516-3223-6-ND HCPL-053L-500E
516-2161-5-ND ACPL-054L-000E
516-4038-2-ND,516-4038-1-ND,516-4038-6-ND HCNR200-500E
516-1608-5-ND HCNR200-300E
516-1627-ND HCPL-0370-000E
516-3683-2-ND,516-3683-1-ND,516-3683-6-ND ACPL-054L-500E
516-4193-2-ND,516-4193-1-ND,516-4193-6-ND HCPL-0370-500E
264-TLX9175J(TPLFTR-ND,264-TLX9175J(TPLFCT-ND,264-TLX9175J(TPLFDKR-ND TLX9175J(TPL,F
516-1545-5-ND HCPL-3700-000E
516-1676-5-ND HCPL-3700-300E
516-3211-2-ND,516-3211-1-ND,516-3211-6-ND HCPL-3700-500E
516-1641-5-ND HCPL-0730-000E
516-4202-2-ND,516-4202-1-ND,516-4202-6-ND HCPL-0730-500E
516-4204-2-ND,516-4204-1-ND,516-4204-6-ND HCPL-073L-500E
559-PS2841-4A-F3-AXTR-ND,559-PS2841-4A-F3-AXCT-ND,559-PS2841-4A-F3-AXDKR-ND PS2841-4A-F3-AX
559-PS2841-4B-F3-AXTR-ND,559-PS2841-4B-F3-AXCT-ND,559-PS2841-4B-F3-AXDKR-ND PS2841-4B-F3-AX
IL300-EF-X009TTR-ND,IL300-EF-X009TCT-ND,IL300-EF-X009TDKR-ND IL300-EF-X009T
516-1535-2-ND,516-1535-1-ND,516-1535-6-ND HCPL-0731-500E
516-1523-5-ND HCNR201-000E
516-1609-5-ND HCNR201-300E
516-1773-2-ND,516-1773-1-ND,516-1773-6-ND HCNR201-500E
516-2379-5-ND HCNR201-050E
516-3916-2-ND,516-3916-1-ND,516-3916-6-ND HCNR201-550E
516-4194-2-ND,516-4194-1-ND,516-4194-6-ND HCPL-0534-500E
516-1677-5-ND HCPL-3760-000E
516-4057-2-ND,516-4057-1-ND,516-4057-6-ND HCPL-3760-500E
516-1743-5-ND HCPL-3760-300E
516-ACPL-K73A-560ETR-ND,516-ACPL-K73A-560ECT-ND,516-ACPL-K73A-560EDKR-ND ACPL-K73A-560E
PVI5080NSPBF-ND PVI5080NSPBF
264-TLX9160T(TPLFTR-ND,264-TLX9160T(TPLFCT-ND,264-TLX9160T(TPLFDKR-ND TLX9160T(TPL,F
751-1296-5-ND IL300-F
IL300-F-X009TTR-ND,IL300-F-X009TCT-ND,IL300-F-X009TDKR-ND IL300-F-X009T
IL300-F-X007-ND IL300-F-X007
751-1294-5-ND IL300-E
365-1909-ND 4N49UTX
365-1853-ND OPI150
3320-OLS300-ND OLS300
3320-OLS910-ND OLS910
2244-OPTO-150-ND OPTO-150
2244-OR-100-ND OR-100
516-1834-5-ND 6N140A
3320-OLS249-ND OLS249
516-2610-5-ND 6N140A#300
3320-OLS449-ND OLS449
516-2171-ND 6N140A/883B
516-2597-5-ND 8302401EA
516-2549-ND HCPL-5731
3320-OLS2449-ND OLS2449
FOD817B300W-ND FOD817B300W
31-DPC817S-C-TR-ND,31-DPC817S-C-TRCT-ND,31-DPC817S-C-TRDKR-ND DPC817S-C-TR
31-DPC817S-B-TR-ND,31-DPC817S-B-TRCT-ND,31-DPC817S-B-TRDKR-ND DPC817S-B-TR
160-1366-5-ND LTV-817
PC817X2NSZ9F-ND PC817X2NSZ9F
732-140357145000TR-ND,732-140357145000CT-ND,732-140357145000DKR-ND 1.40357E+11
732-140357145400TR-ND,732-140357145400CT-ND,732-140357145400DKR-ND 1.40357E+11
732-140100146000TR-ND,732-140100146000CT-ND,732-140100146000DKR-ND 1.401E+11
732-140357145200TR-ND,732-140357145200CT-ND,732-140357145200DKR-ND 1.40357E+11
732-140106146000TR-ND,732-140106146000CT-ND,732-140106146000DKR-ND 1.40106E+11
732-140357145100TR-ND,732-140357145100CT-ND,732-140357145100DKR-ND 1.40357E+11
732-140817143400TR-ND,732-140817143400CT-ND,732-140817143400DKR-ND 1.40817E+11
732-140108146000TR-ND,732-140108146000CT-ND,732-140108146000DKR-ND 1.40108E+11
732-140817143200TR-ND,732-140817143200CT-ND,732-140817143200DKR-ND 1.40817E+11
160-1360-5-ND LTV-816
160-2037-5-ND LTV-817-A
160-LTV-814S-TA1-ATR-ND,160-LTV-814S-TA1-ACT-ND,160-LTV-814S-TA1-ADKR-ND LTV-814S-TA1-A
FOD817D-ND FOD817D
2007-APC-817D1-SLTR-ND,2007-APC-817D1-SLCT-ND,2007-APC-817D1-SLDKR-ND APC-817D1-SL
2007-APC-817B1-SLTR-ND,2007-APC-817B1-SLCT-ND,2007-APC-817B1-SLDKR-ND APC-817B1-SL
2007-APC-817A1-SLTR-ND,2007-APC-817A1-SLCT-ND,2007-APC-817A1-SLDKR-ND APC-817A1-SL
2007-APC-817C1-SLTR-ND,2007-APC-817C1-SLCT-ND,2007-APC-817C1-SLDKR-ND APC-817C1-SL
LTV-817-C-ND LTV-817-C
FOD817B-ND FOD817B
160-1304-5-ND 4N35
160-2038-2-ND,160-2038-1-ND,160-2038-6-ND LTV-817S-TA
160-LTV-816S-TATR-ND,160-LTV-816S-TACT-ND,160-LTV-816S-TADKR-ND LTV-816S-TA
FOD817DS-ND FOD817DS
LTV-817S-B-ND LTV-817S-B
FOD817A3S-ND FOD817A3S
FOD817A300-ND FOD817A300
LTV-817S-D-ND LTV-817S-D
LTV-817S-A-ND LTV-817S-A
FOD817B3S-ND FOD817B3S
VO618A-4X017TTR-ND,VO618A-4X017TCT-ND,VO618A-4X017TDKR-ND VO618A-4X017T
VO617A-3X017TTR-ND,VO617A-3X017TCT-ND,VO617A-3X017TDKR-ND VO617A-3X017T
160-1318-5-ND CNY17F-2
160-LTV-816S-TA1-DTR-ND,160-LTV-816S-TA1-DCT-ND,160-LTV-816S-TA1-DDKR-ND LTV-816S-TA1-D
VO618A-4X016-ND VO618A-4X016
VO617A-ND VO617A
160-LTV-817S-TA1-BTR-ND,160-LTV-817S-TA1-BCT-ND,160-LTV-817S-TA1-BDKR-ND LTV-817S-TA1-B
160-1300-5-ND 4N25
VO615A-8X017TTR-ND,VO615A-8X017TCT-ND,VO615A-8X017TDKR-ND VO615A-8X017T
160-LTV-817S-TA1-CTR-ND,160-LTV-817S-TA1-CCT-ND,160-LTV-817S-TA1-CDKR-ND LTV-817S-TA1-C
VO615A-6X017TTR-ND,VO615A-6X017TCT-ND,VO615A-6X017TDKR-ND VO615A-6X017T
732-140354245000TR-ND,732-140354245000CT-ND,732-140354245000DKR-ND 1.40354E+11
160-LTV-816S-TA1-CTR-ND,160-LTV-816S-TA1-CCT-ND,160-LTV-816S-TA1-CDKR-ND LTV-816S-TA1-C
VO617A-3X007TTR-ND,VO617A-3X007TCT-ND,VO617A-3X007TDKR-ND VO617A-3X007T
732-140814243100TR-ND,732-140814243100CT-ND,732-140814243100DKR-ND 1.40814E+11
732-140356145200TR-ND,732-140356145200CT-ND,732-140356145200DKR-ND 1.40356E+11
732-140354245100TR-ND,732-140354245100CT-ND,732-140354245100DKR-ND 1.40354E+11
VO617A-3-ND VO617A-3
732-140356145400TR-ND,732-140356145400CT-ND,732-140356145400DKR-ND 1.40356E+11
VO617A-4X007TTR-ND,VO617A-4X007TCT-ND,VO617A-4X007TDKR-ND VO617A-4X007T
732-140356145100TR-ND,732-140356145100CT-ND,732-140356145100DKR-ND 1.40356E+11
VO618A-4-ND VO618A-4
VO617A-4X016-ND VO617A-4X016
732-140814242000TR-ND,732-140814242000CT-ND,732-140814242000DKR-ND 1.40814E+11
VO618A-3-ND VO618A-3
160-1302-5-ND 4N26
751-VO618A-3X018TTR-ND,751-VO618A-3X018TCT-ND,751-VO618A-3X018TDKR-ND VO618A-3X018T
VO617A-9-ND VO617A-9
160-1306-5-ND 4N37
FOD817B300-ND FOD817B300
160-1305-5-ND 4N35S
160-1301-5-ND 4N25S
VO615A-9X017TTR-ND,VO615A-9X017TCT-ND,VO615A-9X017TDKR-ND VO615A-9X017T
FOD817-ND FOD817
FOD817CSDTR-ND,FOD817CSDCT-ND,FOD817CSDDKR-ND FOD817CSD
160-1320-5-ND CNY17F-3
FOD817S-ND FOD817S
160-1322-5-ND CNY17F-4
516-1585-5-ND HCPL-817-000E
160-1314-5-ND CNY17-4
160-1312-5-ND CNY17-3
160-1310-5-ND CNY17-2
FOD817CS-ND FOD817CS
160-1308-5-ND CNY17-1
FOD817300-ND FOD817300
FOD817C300-ND FOD817C300
160-1313-5-ND CNY17-3S
BPC-817(BBIN)-ND BPC-817 ( B BIN )
160-1910-2-ND,160-1910-1-ND,160-1910-6-ND 4N25S-TA1
160-1309-5-ND CNY17-1S
160-1913-2-ND,160-1913-1-ND,160-1913-6-ND 4N37S-TA1
2007-BPC-817S(CBIN)TR-ND,2007-BPC-817S(CBIN)CT-ND,2007-BPC-817S(CBIN)DKR-ND BPC-817S ( C BIN )
160-1358-5-ND LTV-815
FOD817C300W-ND FOD817C300W
160-1311-5-ND CNY17-2S
IS357TR-ND,IS357CT-ND,IS357DKR-ND IS357
160-1369-5-ND LTV-827S
160-1359-5-ND LTV-815S
160-LTV-357T-BTR-ND,160-LTV-357T-BCT-ND,160-LTV-357T-BDKR-ND LTV-357T-B
160-LTV-356T-DTR-ND,160-LTV-356T-DCT-ND,160-LTV-356T-DDKR-ND LTV-356T-D
160-LTV-357T-CTR-ND,160-LTV-357T-CCT-ND,160-LTV-357T-CDKR-ND LTV-357T-C
160-LTV-356T-ATR-ND,160-LTV-356T-ACT-ND,160-LTV-356T-ADKR-ND LTV-356T-A
IS181BTR-ND,IS181BCT-ND,IS181BDKR-ND IS181B
IS181DTR-ND,IS181DCT-ND,IS181DDKR-ND IS181D
58-IS357DTR-ND,58-IS357DCT-ND,58-IS357DDKR-ND IS357D
TLP621X-ND TLP621X
PS2501-1X-ND PS2501-1X
FOD817BS-ND FOD817BS
TLP621XGB-ND TLP621XGB
IS181GBTR-ND,IS181GBCT-ND,IS181GBDKR-ND IS181GB
58-ISP521-1X-ND ISP521-1X
58-ISP817A-ND ISP817A
58-TLP521-1X-ND TLP521-1X
160-2242-2-ND,160-2242-1-ND,160-2242-6-ND CNY17-3S-TA
160-1885-2-ND,160-1885-1-ND,160-1885-6-ND CNY17-3S-TA1
160-1344-5-ND LTV-814
FOD817BSDTR-ND,FOD817BSDCT-ND,FOD817BSDDKR-ND FOD817BSD
TLP185(GRH-TLSETR-ND,TLP185(GRH-TLSECT-ND,TLP185(GRH-TLSEDKR-ND TLP185(GRH-TL,SE
TLP291(Y-TPSETR-ND,TLP291(Y-TPSECT-ND,TLP291(Y-TPSEDKR-ND TLP291(Y-TP,SE
TLP291(TPSETR-ND,TLP291(TPSECT-ND,TLP291(TPSEDKR-ND TLP291(TP,SE
TLP185(GRL-TLSETR-ND,TLP185(GRL-TLSECT-ND,TLP185(GRL-TLSEDKR-ND TLP185(GRL-TL,SE
VOM617A-9TR-ND,VOM617A-9CT-ND,VOM617A-9DKR-ND VOM617A-9T
VOM617A-3TR-ND,VOM617A-3CT-ND,VOM617A-3DKR-ND VOM617A-3T
VOM618A-3X001TTR-ND,VOM618A-3X001TCT-ND,VOM618A-3X001TDKR-ND VOM618A-3X001T
264-TLP185(GB-TPR,SETR-ND,264-TLP185(GB-TPR,SECT-ND,264-TLP185(GB-TPR,SEDKR-ND TLP185(GB-TPR,SE
TLP185(GR-TPLSETR-ND,TLP185(GR-TPLSECT-ND,TLP185(GR-TPLSEDKR-ND TLP185(GR-TPL,SE
TLP185(BLL-TLSETR-ND,TLP185(BLL-TLSECT-ND,TLP185(BLL-TLSEDKR-ND TLP185(BLL-TL,SE
VOM618A-3TR-ND,VOM618A-3CT-ND,VOM618A-3DKR-ND VOM618A-3T
TLP185(BL-TPLSETR-ND,TLP185(BL-TPLSECT-ND,TLP185(BL-TPLSEDKR-ND TLP185(BL-TPL,SE
VOM617ATR-ND,VOM617ACT-ND,VOM617ADKR-ND VOM617AT
VOM617A-4TTR-ND,VOM617A-4TCT-ND,VOM617A-4TDKR-ND VOM617A-4T
VOM617A-3X001TTR-ND,VOM617A-3X001TCT-ND,VOM617A-3X001TDKR-ND VOM617A-3X001T
TLP291(GRL-TPSETR-ND,TLP291(GRL-TPSECT-ND,TLP291(GRL-TPSEDKR-ND TLP291(GRL-TP,SE
VOM618A-4TTR-ND,VOM618A-4TCT-ND,VOM618A-4TDKR-ND VOM618A-4T
TLP185(TPLSETR-ND,TLP185(TPLSECT-ND,TLP185(TPLSEDKR-ND TLP185(TPL,SE
751-VOM617A-6TTR-ND,751-VOM617A-6TCT-ND,751-VOM617A-6TDKR-ND VOM617A-6T
160-LTV-217-A-GTR-ND,160-LTV-217-A-GCT-ND,160-LTV-217-A-GDKR-ND LTV-217-A-G
264-TLP185(GR-TPR,SETR-ND,264-TLP185(GR-TPR,SECT-ND,264-TLP185(GR-TPR,SEDKR-ND TLP185(GR-TPR,SE
264-TLP291(V4GBTP,SETR-ND,264-TLP291(V4GBTP,SECT-ND,264-TLP291(V4GBTP,SEDKR-ND TLP291(V4GBTP,SE
VOM618A-8X001TTR-ND,VOM618A-8X001TCT-ND,VOM618A-8X001TDKR-ND VOM618A-8X001T
VOM617A-4X001TTR-ND,VOM617A-4X001TCT-ND,VOM617A-4X001TDKR-ND VOM617A-4X001T
TLP291(SE-ND TLP291(SE
TLP185(SE-ND TLP185(SE
160-1345-5-ND LTV-814S
160-2238-2-ND,160-2238-1-ND,160-2238-6-ND LTV-217-C-G
FOD817C3SDTR-ND,FOD817C3SDCT-ND,FOD817C3SDDKR-ND FOD817C3SD
160-LTV-217-TP1-B-GTR-ND,160-LTV-217-TP1-B-GCT-ND,160-LTV-217-TP1-B-GDKR-ND LTV-217-TP1-B-G
516-3001-ND HCPL-817-00AE
FOD817SDTR-ND,FOD817SDCT-ND,FOD817SDDKR-ND FOD817SD
ISP817XSM-ND ISP817XSM
TLP621XSM-ND TLP621XSM
58-TLP621XGRSM-ND TLP621XGRSM
FOD817ASDTR-ND,FOD817ASDCT-ND,FOD817ASDDKR-ND FOD817ASD
296-ISOM8110DFHRTR-ND,296-ISOM8110DFHRCT-ND,296-ISOM8110DFHRDKR-ND ISOM8110DFHR
TLP183(GR-TPLETR-ND,TLP183(GR-TPLECT-ND,TLP183(GR-TPLEDKR-ND TLP183(GR-TPL,E
TLP184(GB-TPLSETR-ND,TLP184(GB-TPLSECT-ND,TLP184(GB-TPLSEDKR-ND TLP184(GB-TPL,SE
TLP290(GR-TPSETR-ND,TLP290(GR-TPSECT-ND,TLP290(GR-TPSEDKR-ND TLP290(GR-TP,SE
160-1350-5-ND LTV-814H
TLP293(TPLETR-ND,TLP293(TPLECT-ND,TLP293(TPLEDKR-ND TLP293(TPL,E
TLP290(TPSETR-ND,TLP290(TPSECT-ND,TLP290(TPSEDKR-ND TLP290(TP,SE
TLP290(BL-TPSETR-ND,TLP290(BL-TPSECT-ND,TLP290(BL-TPSEDKR-ND TLP290(BL-TP,SE
264-TLP184(TPR,SETR-ND,264-TLP184(TPR,SECT-ND,264-TLP184(TPR,SEDKR-ND TLP184(TPR,SE
TLP293(BLL-TPLETR-ND,TLP293(BLL-TPLECT-ND,TLP293(BLL-TPLEDKR-ND TLP293(BLL-TPL,E
559-1716-ND PS2561A-1-H-A
TLP293(GRH-TPLETR-ND,TLP293(GRH-TPLECT-ND,TLP293(GRH-TPLEDKR-ND TLP293(GRH-TPL,E
TLP184(BL-TPLSETR-ND,TLP184(BL-TPLSECT-ND,TLP184(BL-TPLSEDKR-ND TLP184(BL-TPL,SE
264-TLP184(GB-TPR,SETR-ND,264-TLP184(GB-TPR,SECT-ND,264-TLP184(GB-TPR,SEDKR-ND TLP184(GB-TPR,SE
160-1368-5-ND LTV-827
160-1362-5-ND LTV-826
58-SFH615A-4XSMT&RTR-ND,58-SFH615A-4XSMT&RCT-ND,58-SFH615A-4XSMT&RDKR-ND SFH615A-4XSMT&R
TLP293(BLE-ND TLP293(BL,E
296-ISOM8111DFHRTR-ND,296-ISOM8111DFHRCT-ND,296-ISOM8111DFHRDKR-ND ISOM8111DFHR
58-ISP817XSMT&RTR-ND,58-ISP817XSMT&RCT-ND,58-ISP817XSMT&RDKR-ND ISP817XSMT&R
TLP290(GB-TPSETR-ND,TLP290(GB-TPSECT-ND,TLP290(GB-TPSEDKR-ND TLP290(GB-TP,SE
TLP290(SE-ND TLP290(SE
TLP293(E-ND TLP293(E
FOD814AS-ND FOD814AS
FOD814S-ND FOD814S
516-1878-5-ND HCPL-817-300E
516-2226-2-ND,516-2226-1-ND,516-2226-6-ND HCPL-817-50AE
516-2721-5-ND HCPL-817-30DE
VOS618A-2TTR-ND,VOS618A-2TCT-ND,VOS618A-2TDKR-ND VOS618A-2T
VOS617A-9TTR-ND,VOS617A-9TCT-ND,VOS617A-9TDKR-ND VOS617A-9T
VOS615A-3X001TTR-ND,VOS615A-3X001TCT-ND,VOS615A-3X001TDKR-ND VOS615A-3X001T
VOS617ATTR-ND,VOS617ATCT-ND,VOS617ATDKR-ND VOS617AT
VOS618ATTR-ND,VOS618ATCT-ND,VOS618ATDKR-ND VOS618AT
160-1363-5-ND LTV-826S
751-VOS618A-8X001TTR-ND,751-VOS618A-8X001TCT-ND,751-VOS618A-8X001TDKR-ND VOS618A-8X001T
VOS617A-9X001TTR-ND,VOS617A-9X001TCT-ND,VOS617A-9X001TDKR-ND VOS617A-9X001T
VOS618A-8TTR-ND,VOS618A-8TCT-ND,VOS618A-8TDKR-ND VOS618A-8T
VOS615ATTR-ND,VOS615ATCT-ND,VOS615ATDKR-ND VOS615AT
751-1347-2-ND,751-1347-1-ND,751-1347-6-ND SFH6156-3T
160-1351-5-ND LTV-814HS
VOS615A-4TTR-ND,VOS615A-4TCT-ND,VOS615A-4TDKR-ND VOS615A-4T
VOS615A-2X001TTR-ND,VOS615A-2X001TCT-ND,VOS615A-2X001TDKR-ND VOS615A-2X001T
751-VOS617A-8TTR-ND,751-VOS617A-8TCT-ND,751-VOS617A-8TDKR-ND VOS617A-8T
160-LTV-358TTR-ND,160-LTV-358TCT-ND,160-LTV-358TDKR-ND LTV-358T
559-1071-ND PS2501-1-K-A
TLP182(GB-TPLETR-ND,TLP182(GB-TPLECT-ND,TLP182(GB-TPLEDKR-ND TLP182(GB-TPL,E
559-1072-ND PS2501-1-L-A
1080-EL1017(TA)-VG(DGK)TR-ND,1080-EL1017(TA)-VG(DGK)CT-ND,1080-EL1017(TA)-VG(DGK)DKR-ND EL1017(TA)-VG(DGK)
TLP182(GR-TPLETR-ND,TLP182(GR-TPLECT-ND,TLP182(GR-TPLEDKR-ND TLP182(GR-TPL,E
160-LTV-826S-TA1TR-ND,160-LTV-826S-TA1CT-ND,160-LTV-826S-TA1DKR-ND LTV-826S-TA1
264-TLP292(GR-TPL,ETR-ND,264-TLP292(GR-TPL,ECT-ND,264-TLP292(GR-TPL,EDKR-ND TLP292(GR-TPL,E
264-TLP385(GR-TPL,ETR-ND,264-TLP385(GR-TPL,ECT-ND,264-TLP385(GR-TPL,EDKR-ND TLP385(GR-TPL,E
TLP292(BL-TPLETR-ND,TLP292(BL-TPLECT-ND,TLP292(BL-TPLEDKR-ND TLP292(BL-TPL,E
1080-1602-2-ND,1080-1602-1-ND,1080-1602-6-ND EL814S1(A)(TA)-V
559-1000-ND PS2501-1-M-A
TLP182(TPLETR-ND,TLP182(TPLECT-ND,TLP182(TPLEDKR-ND TLP182(TPL,E
FOD814A-ND FOD814A
FOD8173S-ND FOD8173S
264-TLP385(GB-TPL,ETR-ND,264-TLP385(GB-TPL,ECT-ND,264-TLP385(GB-TPL,EDKR-ND TLP385(GB-TPL,E
FOD814-ND FOD814
4N37MFS-ND 4N37M
VOL617A-4TTR-ND,VOL617A-4TCT-ND,VOL617A-4TDKR-ND VOL617A-4T
FODM121-ND FODM121
VOL617A-4X001TTR-ND,VOL617A-4X001TCT-ND,VOL617A-4X001TDKR-ND VOL617A-4X001T
VOL617A-8X001TTR-ND,VOL617A-8X001TCT-ND,VOL617A-8X001TDKR-ND VOL617A-8X001T
516-1577-5-ND CNY17-4-000E
FODM121A-ND FODM121A
CNY173M-ND CNY173M
516-3176-5-ND HCPL-814-000E
FODM217B-ND FODM217B
FODM121AR2TR-ND,FODM121AR2CT-ND,FODM121AR2DKR-ND FODM121AR2
VOL617A-3TTR-ND,VOL617A-3TCT-ND,VOL617A-3TDKR-ND VOL617A-3T
FODM217A-ND FODM217A
TLP383(GR-TPLETR-ND,TLP383(GR-TPLECT-ND,TLP383(GR-TPLEDKR-ND TLP383(GR-TPL,E
TLP383(D4BLLTLETR-ND,TLP383(D4BLLTLECT-ND,TLP383(D4BLLTLEDKR-ND TLP383(D4BLLTL,E
264-TLP383(D4GB-TL,ETR-ND,264-TLP383(D4GB-TL,ECT-ND,264-TLP383(D4GB-TL,EDKR-ND TLP383(D4GB-TL,E
TLP2301(TPLETR-ND,TLP2301(TPLECT-ND,TLP2301(TPLEDKR-ND TLP2301(TPL,E
TLP620X-ND TLP620X
PS2505-1X-ND PS2505-1X
4N37-ND 4N37
4N28VS-ND 4N28
4N26-ND 4N26
4N36VS-ND 4N36
160-LTV-814-A-ND LTV-814-A
751-TCMT1108TR-ND,751-TCMT1108CT-ND,751-TCMT1108DKR-ND TCMT1108
751-TCMT1102TR-ND,751-TCMT1102CT-ND,751-TCMT1102DKR-ND TCMT1102
TCMT1104TR-ND,TCMT1104CT-ND,TCMT1104DKR-ND TCMT1104
1080-1601-2-ND,1080-1601-1-ND,1080-1601-6-ND EL357N(C)(TA)-VG
FODM2701R2TR-ND,FODM2701R2CT-ND,FODM2701R2DKR-ND FODM2701R2
FODM217D-ND FODM217D
488-FODM217CR2TR-ND,488-FODM217CR2CT-ND,488-FODM217CR2DKR-ND FODM217CR2
FODM217CVOS-ND FODM217CV
HMHA2801-ND HMHA2801
TCMT1119TR-ND,TCMT1119CT-ND,TCMT1119DKR-ND TCMT1119
FODM217DR2OSTR-ND,FODM217DR2OSCT-ND,FODM217DR2OSDKR-ND FODM217DR2
FODM217COS-ND FODM217C
1080-1504-ND EL3H7(A)-G
516-2581-2-ND,516-2581-1-ND,516-2581-6-ND HCPL-181-00DE
559-RV1S2281ACCSP-10YC#KC0TR-ND,559-RV1S2281ACCSP-10YC#KC0CT-ND,559-RV1S2281ACCSP-10YC#KC0DKR-ND RV1S2281ACCSP-10YC#KC0
FODM124R2VTR-ND,FODM124R2VCT-ND,FODM124R2VDKR-ND FODM124R2V
FODM1007R2TR-ND,FODM1007R2CT-ND,FODM1007R2DKR-ND FODM1007R2
516-3761-ND HCPL-814-300E
CNY17G-3-ND CNY17G-3
FODM1009R2TR-ND,FODM1009R2CT-ND,FODM1009R2DKR-ND FODM1009R2
751-1271-5-ND CNY17F-3
751-1268-5-ND CNY17-4
MCT2EM-ND MCT2EM
751-1265-5-ND CNY17-1
HMHA281-ND HMHA281
FODM2705-ND FODM2705
488-FODM217DR2VTR-ND,488-FODM217DR2VCT-ND,488-FODM217DR2VDKR-ND FODM217DR2V
4N35MFS-ND 4N35M
FODM217DVOS-ND FODM217DV
516-2892-2-ND,516-2892-1-ND,516-2892-6-ND ACPL-217-50AE
516-4263-2-ND,516-4263-1-ND,516-4263-6-ND HCPL-181-06BE
516-3135-2-ND,516-3135-1-ND,516-3135-6-ND HCPL-181-06CE
516-ACPL-217-50CETR-ND,516-ACPL-217-50CECT-ND,516-ACPL-217-50CEDKR-ND ACPL-217-50CE
4N35SR2MTR-ND,4N35SR2MCT-ND,4N35SR2MDKR-ND 4N35SR2M
516-4N35-000E-ND 4N35-000E
516-CNY17-3-000E-ND CNY17-3-000E
H11A1SM-ND H11A1SM
516-4N25-000E-ND 4N25-000E
58-H11B2-ND H11B2
58-4N29-ND 4N29
58-4N33-ND 4N33
H11B1IS-ND H11B1
751-4N25-ND 4N25
CNY173SM-ND CNY173SM
TIL111M-ND TIL111M
4N25-X000-ND 4N25-X000
H11A1MFS-ND H11A1M
4N25MFS-ND 4N25M
4N25SR2MTR-ND,4N25SR2MCT-ND,4N25SR2MDKR-ND 4N25SR2M
4N35SM-ND 4N35SM
4N25SM-ND 4N25SM
4N26MFS-ND 4N26M
4N26SR2MTR-ND,4N26SR2MCT-ND,4N26SR2MDKR-ND 4N26SR2M
MOC217M-ND MOC217M
4N36M-ND 4N36M
VOL628A-3TTR-ND,VOL628A-3TCT-ND,VOL628A-3TDKR-ND VOL628A-3T
HMHA2801AR2TR-ND,HMHA2801AR2CT-ND,HMHA2801AR2DKR-ND HMHA2801AR2
732-141355145000TR-ND,732-141355145000CT-ND,732-141355145000DKR-ND 1.41355E+11
HMHA2801A-ND HMHA2801A
516-4264-2-ND,516-4264-1-ND,516-4264-6-ND HCPL-181-06DE
516-3205-2-ND,516-3205-1-ND,516-3205-6-ND CNY17-3-500E
MOC217R2MTR-ND,MOC217R2MCT-ND,MOC217R2MDKR-ND MOC217R2M
751-1367-2-ND,751-1367-1-ND,751-1367-6-ND SFH690ABT
516-ACPL-217-56DETR-ND,516-ACPL-217-56DECT-ND,516-ACPL-217-56DEDKR-ND ACPL-217-56DE
TCLT1000TR-ND,TCLT1000CT-ND,TCLT1000DKR-ND TCLT1000
TCLT1007TR-ND,TCLT1007CT-ND,TCLT1007DKR-ND TCLT1007
1080-EL1018(TA)-VGTR-ND,1080-EL1018(TA)-VGCT-ND,1080-EL1018(TA)-VGDKR-ND EL1018(TA)-VG
HMHAA280-ND HMHAA280
TCLT1006TR-ND,TCLT1006CT-ND,TCLT1006DKR-ND TCLT1006
MOC8050M-ND MOC8050M
MOC205M-ND MOC205M
TCLT1002TR-ND,TCLT1002CT-ND,TCLT1002DKR-ND TCLT1002
LTV-827S-B-ND LTV-827S-B
TCLT1005TR-ND,TCLT1005CT-ND,TCLT1005DKR-ND TCLT1005
160-2254-2-ND,160-2254-1-ND,160-2254-6-ND LTV-214
516-2481-2-ND,516-2481-1-ND,516-2481-6-ND HCPL-354-000E
160-1356-5-ND LTV-8141
160-2039-5-ND LTV-825
TCLT1109TR-ND,TCLT1109CT-ND,TCLT1109DKR-ND TCLT1109