Unimax limit switch

Looking for a replacement limit switch. Unimax skhlo. This is a lever operating 30amp 277vac rated switch. It is in an Onan transfer switch part onan ptn 0308-1166. I replaced these 6 months ago and am not impressed that have high resistance already.

Hello,

Welcome to the TechForum!

I was able to locate some similar options and have them on the link below. I was not able to get as high as the originals 30A rating but thse are as close as we have available.

Thank you
Ryan

thanks Ryan. If this circuit hits 30 amps, there are a lot bigger problems going on. I could see where the contact would be the point of failure, so a 20-25 amp would be more then acceptable.

@andy.stroud

The 480-6236-ND was found.

i looked at the data sheet and the mounting does not fit. Also the lever on my limit switch does not have a simulated roller on it. Just straight blade. my switches have two mounting holes at the top towards the lever. Holes are inline and are aprroximately 24-25mm on center.

I was able to find part number CKN9948-ND as a possible match, would this work for you?

That is close and might work. The common and switched ends are turned around which might take some rewiring but i think i can make it work.