Webinar: Eaton - Beyond Blackouts: How Smart Energy Storage is Changing the Industry

Eaton

Webinar Date: January 22, 2026

Key Takeaways

  • The Growing Challenge: Rising energy demand and aging infrastructure are causing more frequent outages worldwide.
  • Renewable Limitations: Solar, wind, and other alternatives are vital but cannot always meet peak demand without storage.
  • Smart Storage Solutions: Advanced battery systems and modular power packs bridge the gap between generation and consumption.
  • Benefits Beyond Backup: Energy storage improves reliability, supports grid stability, and enables renewable integration.
  • Industry Impact: From homes to factories, smart storage is redefining energy resilience and creating new market opportunities.

Frequently Asked Questions

Why is energy storage becoming so important now?

  • We’re seeing more frequent and longer outages due to aging infrastructure, extreme weather, and higher overall energy demand. Energy storage adds a layer of resilience. It’s not just about having backup power anymore, it’s about stabilizing the grid, supporting renewables, and giving homes and businesses more control over their energy.

How is smart storage different from a generator?

  • Smart storage is automatic, silent, and maintenance-free. It requires no fuel, it’s safe indoors, and it provides clean, stable power instantly. Generators work, but they’re noisy, need fuel—which often runs out during emergencies—and they require regular maintenance. Batteries solve many of those pain points.

What makes a system ‘smart’?

  • A smart system can detect outages instantly, manage the energy flow, recharge from grid or solar, and give you real-time control through an app. It optimizes when one buys or uses energy, so it can save money even when the grid is up.

What exactly is a Virtual Power Plant?

  • A VPP connects thousands of home or commercial batteries using software, so they act as one coordinated power source. For example, in Vermont, Green Mountain Power’s network of home batteries saved around $3 million during peak demand events. It helps the grid and benefits customers at the same time.

How do batteries help with renewable energy?

  • Solar peaks at midday, but demand peaks in the evening. Batteries shift that energy to when it’s needed most. They smooth out fluctuations and reduce reliance on fast-start gas plants, making renewables more reliable.

Are cost and installation still big barriers?

  • They’re improving rapidly. Costs have been dropping, and incentives—like the 30% federal tax credit—help a lot. Installation has also gotten easier with modular, plug-and-play systems. But yes, depending on the region, there can still be policy hurdles.

Is it storage safe? I hear about lithium battery fires.

  • Safety is a top priority. Modern home batteries use LFP chemistry, which is extremely stable. Systems also include advanced Battery Management Systems, redundant sensors, and UL 9540/9540A testing. They’re normally installed outdoors or in ventilated areas, and remote monitoring catches issues early. Statistically, home battery incidents are extremely rare.

Could storage really eliminate large blackouts in the future?

  • Not overnight, but we’re moving in that direction. With microgrids, EV-to-home, AI coordination, and distributed batteries acting together, communities will be able to ‘island’ during grid failures. Over time, blackouts may become short, localized events—if they occur at all.

Is one energy storage preferred over the other?

  • The best choice really depends on the size and type of energy storage you’re dealing with. For large-scale systems, pumped hydro or flow batteries often make the most sense. For smaller setups, lithium-based batteries paired with supercapacitors can be a better fit. Supercapacitors, in particular, respond quickly when charging or discharging and once installed correctly, require virtually no maintenance.

A few years ago, there was talk of using a molten salt battery for larger scale battery storage. I haven’t heard much of it recently, so I wonder if that concept is still being pursued?

  • While lithium-ion remains the consumer standard, molten salt technology is preferred for long-duration energy storage (LDES) due to its safety, non-flammability, and lower cost. Adoption is active among utilities, large-scale energy providers, and heavy industry.

Are home builders buying these systems?

  • Home builders like Lennar are increasingly purchasing and installing energy backup systems as a standard feature rather than an optional luxury.

Please tell us about the latest batteries. Are they lithium-sulfur?

  • Li-S is one of the promising technologies in the battery landscape, but other chemistries are also competing such as Sodium-ion and solid-state batteries.

Referral Webinar Link

If you would like more information from this webinar, please review the details below.

DigiKey Webinar Center

DigiKey TechForum Webinar Posts

1 Like