I have this input (I think it’s a scsi 1 50 pin female) and I want to connect to a computer. Which cable would be needed for that.
We do have SCSI to SCSI cables.
Click here
If that is not the type you were wanting would you be able to indicate the connection type you were looking for on the other end of the cable?
I do need scsi to scsi but I do need to connect two of them to one device. Do you all have anything for that too?
It’s been over 20 years since I even looked at SCSI connections but IIRC, external device cables have only 2 connectors.
Most external devices have 2 SCSI connectors so you can you daisy chain 8 devices using 7 cables. You have to install a terminator plug in the output connector of the last device in the chain..
Hello @PaulHutch,
The last SCSI I touched was an external hard drive. It was $500 (1994 money) for a 500 MB.
Adjusted for inflation, that will purchase a nice computer today.
Sincerely,
Aaron