What are popcorn electronic components?

The term “popcorn” identifies the resistors, capacitors, and inductors that make up a disproportionately large share of electronic components. There is no list of qualifying components. Instead, think of the term as a qualifier that guides component selection toward the most common passive components in use today. These popcorn components are best viewed as a supply chain hedge as they are generally long-lived and available from multiple manufacturers.

Key Takeaways

  • All things being equal, design your circuit to accommodate the popcorn part with as wide a tolerance as possible. Instead of 1%, design to accept a wide range of parts.
  • Popcorn thinking is a design strategy and a hedge against supply chain difficulties: it’s an anti-brittle design practice.
  • Popcorn thinking is a signal reflecting wide part acceptance and maturity.
  • All things being equal, manufacturers are best at producing their highest-volume products.
  • The list of popcorn parts has inertia, but it does change with time. Like real unpopped popcorn, such lists have a long but finite shelf life before going stale.
  • DigiKey’s inventory smooths out the ebb and flow of the manufacturer-to-end-user supply chain.

Author: Aaron Dahlen | MSEE | Senior Applications Engineer, DigiKey
Last update: 12 Aug 2026


Figure 1: Image of popcorn components.

Definition of Popcorn Components

It’s a popcorn component if it can clear most of these bars:

  • Availability: The part is available from multiple manufacturers.

  • Manufacturing maturity: There is an implicit assumption that manufacturers are very good at producing quality parts at high volume. It follows that popcorn parts should be high quality at low cost.

  • High stock levels: Since this is a TechForum post, let’s set the bar assuming DigiKey has over a million units in stock.

  • Design familiarity: The parts represent a template burned into the minds of engineers. It starts with common textbook values and extends into a limited list of “frequently used components.”

  • Selective membership: Not all members of the E series carry the popcorn designation. For example, a 10 kΩ 5% resistor is a classic popcorn component. The E24 series resistors immediately above (11 kΩ) and immediately below (9.1 kΩ) are unlikely to qualify.

  • Cost: Most parts cost a few pennies in quantities of 10,000 and greater. The cost reflects the manufacturer’s experience with the product lines. They are better at working out the bugs on a high-volume production run.

Tech Tip: We are tempted to describe popcorn parts as interchangeable. While this is true in noncritical situations, it sets a dangerous precedent because there will always be circuits that require components with highly specific parameters.

Returning to our original mindset definition, popcorn thinking encourages circuit designers to deliberately design circuitry to accommodate a wide variety of components. Again, this is second-source thinking. It’s a hedge against supply chain failure that will stall the production line.

Relationship to Jellybean Components

Popcorn parts are not the same as jellybean components. Definitionally, jellybean semiconductors are defined in terms of a central classic archetype. For example, the 2N3904 is a central attractor that is over 60 years old. Today, there are hundreds of 3904 variants that share a closely related operating envelope.

By contrast, passive popcorn components are defined as a ubiquitous class of closely related components. For many applications, the popcorn components are interchangeable. There is no canonical ancestor for a component such as a 10 kΩ 5% resistor in an 0805 surface mount package.

Tech Tip: For your next technical trivia game, be sure to ask what value appears in every E series from E3 to E192. The answer is 1 because it is the series anchor (normalized starting value). It is the quintessential popcorn value.

Setting Expectations with a Historical Example

History carries parallel lessons that apply to popcorn thinking. Let’s go all the way back to 1945 to the ENIAC computer. This machine used around 18,000 vacuum tubes which is still an extraordinary number of hand-constructed components. Legend tells how the engineers selected the tubes. Instead of selecting specialized tubes for computer service, they asked the manufacturers to identify the most reliable tubes.

Surprisingly, they were advised to use the most common tubes of the era such as 6SN7, 6SJ7, 6V6, and 6L6 (6V6 tubes shown in Figure 2). This landmark computer used the same tubes that people used for their home radios. These were also the same tubes mass-produced for the war effort. The selection process was very simple. These were the tubes most familiar to the manufacturer. The production lines were established and the bugs had largely been worked out after producing millions of devices.

The same ideas extend to popcorn components. Like the vacuum tubes, all things being equal, mature passive components with high production runs have the lowest cost and highest reliability. Simply stated, manufacturers are best at producing their highest-volume products.

Figure 2: Progression of 6V6 tubes from metal can to button-base.

How to Determine the “Popcorn” Status of a Component

I’d love to share the DigiKey sales data with you. The popcorn qualification answers would be crystal clear. However, that data is sensitive and unlikely to be released. Instead, we need to look at proxy data:

  • Stock quantity: We can assume that inventory level is a proxy for sales volume. An example is shown in Figure 3 where we see the availability of 1 kΩ 1/4 W carbon film resistors with a 5 % tolerance. DigiKey does not purchase these parts simply to have them on hand. They are purchased to sell. A large inventory is a cushion for the customer because DigiKey’s inventory smooths out the ebb and flow of the manufacturer-to-end-user supply chain. Also, there are shelf-life pressures for many components.

  • CAD programs: Tools such as Altium Designer include an Active BOM. This provides DigiKey’s real-time stock availability as the parts are being selected in the schematic designer.

  • Inclusion in the E3 series: Recall that the E series identify preferred values for each decade. For example, the E3 series capacitors are generally available in 1.0, 2.2, 4.7, 10, 22, 47 µF, and so on. As strange as this sounds, these century-old values are deeply embedded into our modern practices. As evidence, ask yourself what is the most commonly cited resistance used for a microcontroller driving an LED? Depends who you ask, but chances are high it’s 220, 470, or 1 kΩ with a few that may point to 330 Ω. Note that 330 Ω is part of the finer E6 series.

  • Textbooks: Our textbooks are an extension of E series thinking. Suppose you are outfitting a lab and need to cover a wide range of resistance values while choosing the minimum total number of resistor values. This optimization naturally leads back to the E3 series. Some will choose up to the E12 series, but rarely go further. Consequently, the 1 kΩ resistor and the 10 µF capacitor are common. Authors rarely specify parts such as 1.05 kΩ or a 6 µF capacitor.

  • Application notes and reference designs: As you review the manufacturer’s materials, you will see the same values over and over again. For example, what is the value of the ceramic bypass capacitor commonly used for integrated circuits? If in doubt, use 0.1 µF. By the way, DigiKey has nearly 50 million of these capacitors in stock (07 Aug 2026). The 0.1 µF capacitor gets my vote for THE most popcorn of popcorn components.

Tech Tip: Let’s address an E-series misunderstanding. The century-old E3 series components do not have the same tolerance as today’s components. In fact, an old 1 µF capacitor may have a tolerance as broad as 40%. This is the natural result of the binning process and the fact that many consumer-grade devices could tolerate the wide tolerance. Today’s parts are often available with a 1% or better tolerance.

There are two competing ideas woven into this engineering brief:

  • Purchase low-cost modern components with a tolerance that fits the performance and cost requirements of your design. As a practical statement, components converge to a 5% tolerance.
  • Design so that you are not dependent on this tolerance. Think in terms of 20% or even 40% if possible. This maximizes future parts availability.

Figure 3: DigiKey parts availability for 1 kΩ 1/4 W carbon film resistors (captured on 07 Aug 2026).

About This Author

Aaron Dahlen, LCDR USCG (Ret.), is a Senior Applications Engineer at DigiKey in Thief River Falls. His background in electronics and industrial automation was shaped by a 27-year military career as both technician and engineer, followed by over a decade of teaching.

Dahlen holds an MSEE from Minnesota State University, Mankato. He has taught in an ABET-accredited electrical engineering program, served as coordinator of an electronic engineering technology program, and instructed military technicians in component-level repair.

Today, he has returned to his home in northern Minnesota, completing a decades-long journey that began with a search for capacitors. Read his story here.