Question:
What do VDC and VAC on the relay case indicate?
![]()
Answer:
VDC is the DC coil voltage and VAC is the AC coil voltage. For example:
G2R-24 24VDC: G2R-24 DC24 is the proper model name.
G2R-24 24VAC: G2R-24 AC24 is the proper model name.
![]()
Explanation:
Shown below is an example of the relay indication of G2R.
Quick tips
When more than one relay voltage is used, check the voltage specification indicated on the case before use.
![]()
Please visit the link below to see this product line on the Digi-Key website
Relays | Digi-Key Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/relays/FAQE10008