I have a 1K resistor (pnCF14JT1KOOCD-ND) that is in a breadboard at location A2 to A10 on a solderless breadboard.
I purchased a DigiKey PN: Solder Breadbox1-kit-nd. There is no A2 on that board because of the holes to locate the board in the box. What pin location can I use instead of A2?
Thanks
Amy
What is the equivalent of the pin location of a2 on a solderless breadboard with the digikey solderb
B2 through E2 all connect to the same copper track as the missing A2 would connect to. So you can use any of those locations as a substitute.
1 Like
Thank you. I thought that might be the case.