What is the failure rate P level on the datasheet of the mechanical relay?

Question:

What is the failure rate P level on the datasheet of the mechanical relay?

Block

Answer:

The P level (reference value) indicates that a failure is expected to occur once in every 10 million cycles in the event of a microload as specified in JIS C 5003.

Block

Explanation:

Contact resistance may be a problem when opening and closing microloads.
If a high contact resistance value is accidentally generated, it may be recovered by the subsequent operation.
In addition, contact resistance may increase due to generation of contact coating.

Whether or not the contact resistance value is considered a failure depends on whether or not a problem occurs in the circuit. For this reason, the failure criteria for the contact resistance of relays are specified only in the initial value, and the failure rate is expressed using the P level (reference value) as a guideline for the minimum applied load.

The failure rate is the rate at which a failure occurs within a unit time (number of operations) when the relay is opened and closed continuously at the specified test type and load.
This value can vary depending on the frequency of opening and closing, the environment, and the level of reliability you expect. Be sure to test the actual equipment under actual operating conditions.

Failure rate

Block

Quick tips

When used at a microload level, the reliability may vary depending on the contact material and contact method. Consider signal (communication) relays that emphasizes contact reliability.

Block

Please visit the link below to see this product line on the Digi-Key website
Relays | Digi-Key Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/relays/FAQE10032