Question:
What is the product life of DIP switches?
Answer:
The electrical durability (life) of DIP switches is more than 1,000 times for sliding type and more than 5,000 steps for rotary type (2,000 steps for A6A and A6C/CV types). Note that improper handling may often lead to shorter product life and/or damage. Please note soldering conditions and the direction of force applied to the operation part.
Explanation:
Shown below is a list of electrical durability (life) of each model. It is indicated by operation count for sliding type and step count (number of times to move one step) for rotary type.
Quick tips
Make sure to use the product properly. In actual use, the product may break earlier than its electric durability due to damage by excessive force, and/or it could have a shorter product life due to internal deformation caused by improper operation direction.
Examples of problems caused by applying the excess force to the actuator can be found on The SOLUTIONS [Operation Switch], which shows “Mechnism of failure occurrence” and"Checkpoint for prevention".
Product category
Switches DIP Switches
Classification
Trouble shootings
Related keywords
DIP Switch
Electrical Durability
Life
Sliding Type
Rotary Type
Operating Count
Step Count
Excess Force
Failure Case
Prevention
Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
What is the product life of DIP switches? | FAQ | OMRON Device & Module Solutions - Americas