Question:
What kind of switch is a tactile switch?
![]()
Answer:
A tactile switch is a switch whose operation is perceptible by touch. These small-sized switches are placed on PCBs and used to close an electrical circuit when someone presses the button. When the button is pressed, the switches turn ON and when the button is released, the switches turn OFF.
![]()
Explanation:
The two types of tactile switches are standard and sealed. The basic structure is as follows:
Standard type
-
Cover
The cover is utilized along with the base to protect the internal mechanisms of the switch. It is made by pressing a metal plate. -
Plunger
The plunger relays the force of the person pressing the switch to the contact dome. It is generally made of resin, but sometimes rubber is used for larger strokes. -
Contact dome
The contact dome is a circular part made of metal. It reverses when force is applied, and allows current to flow between the contacts to turn the switch ON. When the force is removed, the contact dome returns to its original shape and the switch turns OFF. -
Base
The base is made of resin and both the contacts and terminals are combined into a single component to which all other components of the switch are attached. -
Contacts/terminals
Contacts/terminalsThere are two types of terminals: those inserted into through holes on a PCB and those mounted on the surface of a PCB.
Sealed type
-
Cover
The cover is utilized along with the base to protect the internal mechanisms of the switch. It is made by pressing a metal plate. -
Pushbutton
The pushbutton is the resin component that is pressed by a person. The force it receives from a push is relayed to the plunger through the film. -
Film
The film is a thin resin sheet. It seals the contact dome and contacts to prevent any moisture or foreign objects from reaching these components. This component is required to seal the switch. -
Plunger
The plunger relays the force received through the film to the contact dome and causes it to reverse. -
Contact dome
The contact dome is a circular part made of metal. It reverses when force is applied, and allows current to flow between the contacts to turn the switch ON. When the force is removed, the contact dome returns to its original shape, and the switch turns OFF. -
Base
The base is made of resin and both the contacts and terminals are combined into a single component to which all other components of the switch are attached. -
Contacts/terminals
There are two types of terminals: those inserted into through holes on a PCB and those mounted on the surface of a PCB.
For more information, see “What is a Tactile Switch?”
![]()
Product category
Switches Tactile Switches
Classification
Selection, Characteristics
Related keywords
Tactile Switch
Tact Switch
Structure
Sealed Type
Plunger
Contact Dome
![]()
Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/switches/FAQE20058