Question:
Can a tactile switch be used instead of a pushbutton switch?
![]()
Answer:
The prime difference between a pushbutton switch and a tactile switch is rating(resistive load). if the specified rating is met, it is possible to use a tactile swith with the operating precautions shown in Explanation below.
![]()
Explanation:
Although pushbutton switches and tactile switches perform the same function, their structures are very different. Some cautionary tips to follow if using tactile switches in the same way as pushbutton switches:
The equioment structure must be designed so that pushing in the tactile switch should be limited. Pushing in the switch with excessive force may degrade the contact dome and/or damage the switch.
A structure that pushes the center of the operation part is desirable. Pushing in the switch diagonally may lead to shorter product life and damage it.
Keeping the switch pushed in may lead to shorter product life and must be avoided.
![]()
Product category
Switches Tactile Switches
Classification
Usage, Applications
Related keywords
Tactile Switch
Pushbutton Switch
Damage
Product Life
Pushing Diagonally
Contact Dome Damage
Plunger Damage
![]()
Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ
Video on Topic
Here is a video that discusses this topic below.