Question:
What kind of problems may occur if the set current is below the “minimum applicable load” for a basic switch?
![]()
Answer:
Below the minimum applicable load for a basic switch, the contact surface is more susceptible to the chemical coating formed due to the influence of the surrounding environment, leading to potential contact failure.
![]()
Explanation:
The “minimum applicable load” described in the datasheet is the load condition that is confirmed to be opened and closed at the reliability N level, and is not the guaranteed value.
Durability is affected not only by load conditions such as current and voltage but also by the operating environment and stroke settings.
Please evaluate it based on the environment, actual equipment and actual load before deciding whether to use the switch.
![]()
Product category
Switches Basic Switches
Classification
Usage, Applications
Related keywords
Basic Switch
Minimum Applicable Load
Contact Failure
Reliability N Level
Durability
![]()
Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below toview the original FAQ