------Question for CP1E-E10DR-A Please Put your question below------
Hi, it is stated that the OMRON CP1E-E10DR-A PLC input pins are digital, what does it mean? 5VDC input or 24VDC input or 240VAC inputs?
------Question for CP1E-E10DR-A Please Put your question below------
Hi, it is stated that the OMRON CP1E-E10DR-A PLC input pins are digital, what does it mean? 5VDC input or 24VDC input or 240VAC inputs?
Hello @irfan
Welcome to TechForum community!
The input pins on the OMRON CP1E-E10DR-A PLC are digital, which means they should be designed to detect ON/OFF signals.
According to the datasheet page number 27, these inputs operate at 24 VDC (±10% / −15%).
So, to clarify:
Input type: “Normal inputs”
Input voltage: 24 VDC ±10% / −15%
Hi @aayushi.nainwal ,
Thanks for the clarification.