Which LoRa gateway is able to de-modlate the LR-FHSS packet?

Which LoRa gateway is able to de-modlate the LR-FHSS packet? Please give me a link to buy it.

I already bought SX126x and I am able to transmit LR-FHSS packets using a driver.

This is the information that I know about LoRa gateway that satisfied my requirement.

“LR-FHSS demodulation can be achieved on the LoRa® Gateway V2 reference design with external DSP capabilities. LoRa® 16-channel and 64-channel reference designs are available.
The current reference design uses Semtech SX1388 FPGA and OMAPL138 DSP. LoRa 16-channel reception is supported by the two SX1301 baseband processors. Up to 64 channels are supported by the add-on board with additional baseband processors”

Thank you

Hello @jumanamirza,
I am still doing some checking but at this time I have not been able to identify any LoRa gateways we carry that support decoding LR-FHSS packets. I have also done some general searching on the internet and haven’t been able to find any gateways supporting LR-FHSS.

Thank you so much.
Kindly, how can i upgrade firmware of SX1302 gateway to v2?

Hello @jumanamirza,
I am not aware of any firmware to change a SX1302 gateway to LR-FHSS. The only information I have been able to find are some example demos and drivers on GitHub - Lora-net/SWDM001: Long-Range Frequency Hopping Spread Spectrum (LR-FHSS) transmission demo.

Hello @ScottRaeker @jumanamirza ,
I noticed that this conversation is over a year old, but I still cannot find a solution or product related to the topic discussed here.

Do you have any updates regarding a LoRa gateway that can demodulate LR-FHSS packets?

I have found the following information:

  1. “LR-FHSS demodulation will be supported on Semtech SX1301-based V2.1 gateway” from this source: Semtech Blog
  2. “Gateway 2.1 Reference Design LoRa gateway reference design with LR-FHSS capability” from this source: Semtech Salesforce

However, I still cannot locate the Gateway 2.1 reference design or firmware update anywhere. Do you have any idea where I can find it? Or, do you have any other solutions for creating a gateway that supports LR-FHSS demodulation?