Which revision of Terasic P0431 is sold by DigiKey?

------Question for P0431 Please Put your question below------

Terasic has revB and revC versions of the P0431 HDMI-FMC card. The revC board uses the MAX10 level shifter instead of the MAXII level shifter and supports 1.2V I/O.

Which version of the card does DigiKey have in stock? The difference can clearly be identified by looking at the large chip in the center of the card. If it says “MAX 10” then it is the revC board.

Thank you!

Hi malyn, Welcome to the DigiKey TechForum,

DigiKey is unable to provide part specific details of stock prior to shipment. If there are any special requirements for your order such as a specific revision, please include them into the order notes and DigiKey will attempt to accommodate. If we cannot fulfill your order, someone from our customer service dept will contact you.