Hello,
I have a 1738-FIT0817-ND and I wanted to use it for some motor driver types. Um, are they powered via 3.3v, 5v, and/or maybe 12 or 24v?
I can probably use the extra fan consumption during specific moves on my machine but I know exactly nothing about it nor do I have the wherewithal to actually test it properly.
I can start w/ 3.3v and move up to 5v and so on…until it breaks.
Seth
P.S. Should I contact DFRobot instead? Please guide me on this effort so I can make a wiser decision than I have made in the past.
SPECIFICATION
Working Voltage: 5V
Power: 1.5W
Speed: 7500rpm
Weight: 12g
Applicable to 3B/3B+/4B
Size:
Large Heat Sink: 50*25*13mm / 1.97*0.98*0.51 inch
Small Heat Sink: 9*9*5mm / 0.35*0.35*0.2 inch
This is what I found on their DFRobot site online. So, I will go w/ it! Pray for rains!