Hi,
I need to select a connector, something like Molex 0513532400 for 24 circuits but some of my wires are 32 AWG and there is no crimp terminal for that that I see. I need to put wires in this from 32 to 20 AWG. Can you suggest something similar to Molex 0513532400 but which has crimp terminals for wires (doesn’t have to be a single terminal) 32 to 20 AWG? I prefer smallest pitch and 3A min current per pin.
If there are higher rated contacts I can go down to a 20 or 18 circuit connector.
Any suggestions for a connector and terminals which can work on my range of wires?
thanks