205F and 205M circular connector

Hello,

I am looking for these circular connectors that comes attached to this limit switch D4C-442B-A3.

There are two wires coming out of the ends, the red wire has a circular connector with 205M and black wire has a circular connector 205F written on them.

I have attached images of these connectors.

I did purchase the below connectors but it did not work.

0003092011 x2

0002092118 x1

0002091119 x1

Any help would be greatly appreciated!

Hello @rsyed,

Thank you for contacting DigiKey and welcome to the TechForum community.

Part number D4C-442B-A3 does not appear to be a standard model from the D4C series from Omron. I am not sure what the connector or contact part numbers which are used with this part.

I would suggest contact the original OEM this part came from for assistance to see if they can offer connector and contact part numbers.

I’ve already tried contacting the OEM, not really getting anything back from them.

The images that I provided of the connectors, won’t help?

Those would look more akin to something in the family of barrel/bullet style crimp terminals. There’s a degree of informal interoperability among such products if one can pick a suitable size.

Also, such a connector would not seem typical for the D4C switch family, and may well have been an add-on item at some point.

yea the D4C family does not have this connector. The connector appears to be installed later on. I’ve searched through the barrel/bullet style crimp terminals, and no luck..