24v dc 285-300rpm motor

Hi Guys,

How are you going? I have a question I am on the search for a new little motor for one of our cleaning robots the we currently have. I’ll attached a couple of photos so you can see the type of motor. I was hoping you guys would have something similar and be able to help out.

We are on the look to upgrade our small 24v dc motor which produces 180rpm to something a little bigger 24V dc motor @ 280-300RPM would you have something similar?

Hello xtremesolarcare,

Welcome to the DigiKey TechForum! Unfortunately it appears as if the photos did not attach as intended. I’ve assumed the motor is for the sweep and not the wheels, so sorted the parameters to 24VDC with the RPMs being near what your target is and was about to come up with the following:

Note that size, wiring, and torque can all play a role in the motor’s function so you will want to consider that when choosing a motor.

Regards,
Klint