Trying to source a motor(s)

Hi I am trying to source 2 different motors and i wondered if you might be able to help or if DigiKey stock something similar.

Motor 1 = RS550-24V_RPM-12000 (quantity = 4)

Motor 2 = RS390-24V_RPM-6000 (quantity = 1)

I wondered if you stocked these products and if not can i replace them with something similar. The RS550 motor are drive motors for wheels on a childrens electric buggy while the RS390 is the steering drive motor.

Looking forward to hearing from you.

Vinny

Images of both motors are below:

Hello vinny.croke,

Welcome to the DigiKey TechForum.

I’m sorry, but we do not have matches to these motors.

The only thing that came up when searching the 24V, and the 6000 and 12000 RPM, is part number 2790-NF213G-302-ND, which is 6000 RPM, but would be way too small in size.