Replacement for old 12 VDC motor

I had an application that used a:
Micron 31600 3N5144 12 VDC motor
but also used a:
Mocron 31600 3E4534 12 VDC motor
10 yrs ago I couldn’t find either of these so I substituted a:
Nichibo Taiwan MP5-18105AS-R 12 VDC motor.
Now I can’t find either of these. Can you suggest an alternative please?
I can’t find the specs for the Micron motors. The Nichibo was listed as 6545 rpm, 0.63A, 60.5 g/cm torque, 1.05" diameter, 1.25: length, 0.4"-0.5" shaft length, 2mm shaft dia.,0.35" shaft hub
thanks,
John

@usoswalds

The below link shows the 12vdc ~6545rpm motors I had found. I am sorry to say that I am not seeing that we list an option that would also handle the torque spec as well.
Motors - AC, DC | Electronic Components Distributor DigiKey

1 Like

thx Nathan!