Hi
Pls share the AC input voltage of this Part# 9206B ?
It is 110 or 220 VAC ?
Hello @order,
This is an interesting solution. According to the user manual, there is a selector switch on the bottom of the power supply.
Note the warning to set it correctly as this type of damage will “void all warranty.”
Sincerely,
APDahlen
Hello @order,
Does the power supply have a line voltage selector switch on the bottom of the instrument?
Here is a picture from a related B&K instrument.
Sincerely,
Aaron
Note that the warning label reads “Set to 110V AC”.
“Set to . . .” is synonymous with “Configured for . . .”.
This is just to alert you that if you intend to power it with 220V AC, you need to reconfigure it for 220V AC before applying power by sliding that switch on the bottom of the unit that @APDahlen has shown.
Also note that in the manual, they recommend changing the fuse to a T10A type for 220V AC operation. If this fuse is not changed to the lower 10A value, the unit will not be adequately protected under high load conditions.