Agilex™ 3 SoC FPGA Development Kit

Getting Started: Agilex™ 3 SoC FPGA – Hardware Bring Up Guide:

1. Unboxing and Handling

Remove the development kit from the box and place it on an ESD-safe work area.
Use an anti-static mat with proper grounding before handling the board.

Ensure all items are received without any physical damage.

Kit Contents:

  • Agilex™ 3 SoC FPGA (M16A) SOM Development Platform
  • 12V, 5A Power Supply
  • USB Debug Cable

2. Boot Switch Configuration

Ensure the onboard boot switch (SW4) is set correctly as shown in the reference image below.

Refer to the configuration selection truth table for correct boot mode settings.

3. Debug Port Connection

Connect the USB cable as follows:

  • Type-A end → PC
  • Type-C end → Debug USB Type-C connector (J8) on the board

4. JTAG Connection

The M16A SOM supports JTAG interface for FPGA programming and debugging.

Use an Intel USB-Blaster to connect the carrier board. Ensure Switch-3 on the carrier board is turned ON.

Recommended USB-Blaster:

  • Intel USB Blaster-2 (PL-USB2-BLASTER)

5. Powering ON the Board

Connect the 12V power supply to connector J2 and switch ON the power.

Once powered, the board power LED should turn ON.

6. Test Environment Setup

After power-up and hardware connections, verify the system using the debug console and basic test environment setup as per the development guide.

For more details on the Agilex™ 3 development kit, refer below:
iG71D-W135B6-4L002G-E032G-CAA iWave Global | Embedded Complex Logic (FPGA, CPLD) Evaluation Boards | DigiKey

1 Like